Dear Engineer,
To avoid the jitter issue caused by the ADV7280 I2P function, I disabled the I2P function and used the downstream RV1126B to perform de-interlacing. Now I find that with CVBS input, there is a disturbance phenomenon, while S-video input shows no disturbance. I also verified with the internal test pattern using REG0x14's FREE_RUN_PAT_SEL(100% color bars/Luma ramp/Boundary box), and there was no disturbance. How can I optimize the disturbance issue specifically for CVBS input?