Post Go back to editing

ADV7280A: Unstable chroma on first active line of BT.656 (STANAG Class C / NTSC)

Thread Summary

The user encountered unstable chroma artifacts on the first active line of NTSC fields when using the ADV7280A with STANAG 3350 Class C composite input and 8-bit embedded BT.656-4 output. The issue was resolved by changing the VBI-to-active-line controls (registers 0xEB and 0xEC) to 0x05, which stabilized the chroma on the first active line without affecting the BT.656-4 output timing.
AI Generated Content
Category: Hardware

Hello,

I am using the ADV7280A with a STANAG 3350 Class C (NTSC RS-170A timing equivalent) composite input and 8-bit embedded BT.656-4 output.

Symptom:
The first active row of one field shows blinking colored dots (unstable chroma) on saturated colors such as SMPTE bars. Luma appears stable. Row 1 and the following rows are clean.

Isolation:
We checked the raw BT.656 output directly with an FPGA Integrated Logic Analyzer (ILA). The ADV7280A outputs 487 active lines, and the chroma variation is already present on the first active line of the raw byte stream before our FPGA crops it to 720x486 lines for the downstream modules.

Attempted fixes:
We tested several documented registers and EngineerZone-recommended initialization sequences, including 0x27, 0x2B to 0x2E, 0x3D, 0x38 to 0x39, and 0xEB to 0xEC, without any change to the first-line behavior. We have also checked with different video sources.

For reference, our baseline ADV7280A configuration is:
0x00 = 0x00
0x02 = 0x14
0x03 = 0x0C
0x04 = 0xBD
0x1D = 0x64
0x0F = 0x00
0x3A = 0x07

Questions:

1. Is this a known ADV7280A behavior for STANAG Class C / non-broadcast NTSC sources, specifically on the first active line of a field?

2. Could this be related to NTSC field-boundary / SCH burst phase behavior, or to how the ADV7280A handles chroma decoding / comb filtering on the first active line?

3. Is there any documented or undocumented register sequence that can improve first-line chroma stability, or is the recommended approach simply to mask this line downstream?

Thanks in advance for the support.

Kind regards,
Jonathan

Parents
  • ;;DecoderLegacySupport = True;;
    ;;Reset = False;;
    ;;ReadInterface = True;;
    
    ##ASettings##
    :Customer Version 5.0 August 2017 ADV7280A :
    End
    
    ##01_Free-run Mode##
    
    :Free-run, 480i 60Hz YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS 
    42 00 07 ; ADI Required Write [INSEL set to unconnected input]
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :Free-run, Color Bars 480p YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS 
    42 00 07 ; ADI Required Write [INSEL set to unconnected input]
    42 0C 37 ; Force Free run mode
    42 02 54 ; Force standard to NTSC-M
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 80 51 ; ADI Required Write 
    42 81 51 ; ADI Required Write 
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder writes begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :Free-run, 576i 50Hz YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS 
    42 00 07 ; ADI Required Write [INSEL set to unconnected input]
    42 0C 37 ; Force Free run mode
    42 02 84 ; Force standard to PAL
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :Free-run, Color Bars 576p YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS 
    42 00 07 ; ADI Required Write [INSEL set to unconnected input]
    42 0C 37 ; Force Free run mode
    42 02 84 ; Force standard to PAL
    42 14 11 ; Set Free-run pattern to 100% color bars
    42 80 51 ; ADI Required Write 
    42 81 51 ; ADI Required Write 
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    ##02_CVBS AUTODETECT##
    
    :Autodetect CVBS Single Ended In Ain 1, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :Autodetect CVBS Single Ended In Ain 2, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :Autodetect CVBS Single Ended In Ain 3, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :Autodetect CVBS Single Ended In Ain 4, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder writes begin]
    56 01 00 ; Set Encoder to SD mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    ##03_CVBS INTERLACED TO PROGRESSIVE##
    
    :I2P - NTSC In Ain1,YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder writes begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - PAL In Ain1, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - NTSC In Ain2,YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder writes begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - PAL In Ain2, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - NTSC In Ain3,YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder writes begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - PAL In Ain3, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - NTSC In Ain4,YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder writes begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - PAL In Ain4, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    ##04_CVBS FAST Switch##
    
    :FAST Switch CVBS Single Ended In Ain1, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :FAST Switch CVBS Single Ended In Ain2, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :FAST Switch CVBS Single Ended In Ain3, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :FAST Switch CVBS Single Ended In Ain4, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, ped on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    ##05_CVBS FAST Switch I2P##
    
    :I2P FAST SWITCH NTSC Single Ended In Ain1, YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH PAL Single Ended In Ain1, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 00 ; CVBS in on AIN1
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset  [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH NTSC Single Ended In Ain2, YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH PAL Single Ended In Ain2, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 01 ; CVBS in on AIN2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset  [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH NTSC Single Ended In Ain3, YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH PAL Single Ended In Ain3, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 02 ; CVBS in on AIN3
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset  [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH NTSC Single Ended In Ain4, YPbPr Out (480p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P FAST SWITCH PAL Single Ended In Ain4, YPbPr Out (576p EAV/SAV):
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 52 CD ; AFE IBIAS
    42 00 03 ; CVBS in on AIN4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1] 
    42 9C FF ; Reset Current Clamp Circuitry [step2] 
    42 0E 00 ; Enter User Sub Map
    42 0E 80 ; ADI Required Write [Fast Switch]
    42 D9 44 ; ADI Required Write [Fast Switch]
    42 0E 40 ; Select User Sub Map 2 [Fast Switch]
    42 E0 01 ; Select fast Switching Mode [Fast Switch]
    42 0E 00 ; Select User Map [Fast Switch]
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 17 41 ; Enable SH1
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ, HS & VS pads
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write [ADV7280A VPP writes begin]
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes finished]
    56 17 02 ; Software Reset  [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    ##06_YC AUTODETECT##
    
    :YC In Ain1,2, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS 
    42 00 08 ; INSEL = YC, Y - Ain1, C - Ain2
    42 0E 80 ; ADI Required Write
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [All ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, pedestal on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    :YC In Ain3,4, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS 
    42 00 09 ; INSEL = YC, Y - Ain3, C - Ain4
    42 0E 80 ; ADI Required Write
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [All ADV7280A writes finished]
    56 00 1C ; Power up DACs and PLL [Encoder Writes Begin]
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, pedestal on, PbPr SSAF on, YPbPr out
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    ##07_YC INTERLACED TO PROGRESSIVE##
    
    :I2P YC In Ain1,2, 480p EAV/SAV, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS
    42 00 08 ; INSEL = YC, Y - Ain1, C - Ain2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P YC In Ain1,2, 576p EAV/SAV, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS
    42 00 08 ; INSEL = YC, Y - Ain1, C - Ain2
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P YC In Ain3,4, 480p EAV/SAV, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS
    42 00 09 ; INSEL = YC, Y - Ain3, C - Ain4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P YC In Ain3,4, 576p EAV/SAV, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes begin]
    42 53 CE ; AFE IBIAS
    42 00 09 ; INSEL = YC, Y - Ain3, C - Ain4
    42 0E 80 ; ADI Required Write 
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 17 02 ; Software Reset [Encoder Writes Begin]
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End 
    
    ##08_YPbPr AUTODETECT##
    
    :YPbPr In Ain1,2,3, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes Begin]
    42 54 C0 ; AFE IBIAS
    42 00 0C ; INSEL = YPbPr, Y=Ain1, Pb=Ain2, Pr=Ain3
    42 0E 80 ; ADI Required Write
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver [All ADV7280A writes Finished]
    56 00 1C ; Power up Encoder
    56 01 00 ; SD only mode
    56 80 10 ; SSAF Luma filter enabled, NTSC mode
    56 82 C9 ; Step control on, pixel data valid, pedestal on, PbPr SSAF on, YPbPr out.
    56 87 20 ; PAL/NTSC autodetect mode enabled
    56 88 00 ; 8 bit input enabled [Encoder Writes finished]
    End
    
    ##09_YPbPr Interlaced to Progressive##
    
    :I2P - YPbPr In Ain1,2,3, 480p EAV/SAV, YPbPr Out
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes Begin]
    42 54 C0 ; AFE IBIAS
    42 00 0C ; INSEL = YPbPr, Y=Ain1, Pb=Ain2, Pr=Ain3
    42 0E 80 ; ADI Required Write
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map 
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 00 1C ; Power up Encoder
    56 17 02 ; Reset Encoder
    56 00 9C ; Power up DAC's and PLL
    56 01 70 ; ED at 54MHz input
    56 30 04 ; 525p at 59.94 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    :I2P - YPbPr In Ain1,2,3, 576p EAV/SAV, YPbPr Out:
    delay 10 ; Wait 10ms After Hardware Reset To Start I2C
    42 0F 80 ; Reset ADV7280A
    56 17 02 ; Reset Encoder
    delay 10 ; Wait 10ms 
    42 0F 00 ; Exit Power Down Mode [ADV7280A writes Begin]
    42 54 C0 ; AFE IBIAS
    42 00 0C ; INSEL = YPbPr, Y=Ain1, Pb=Ain2, Pr=Ain3
    42 0E 80 ; ADI Required Write
    42 9C 00 ; Reset Current Clamp Circuitry [step1]
    42 9C FF ; Reset Current Clamp Circuitry [step2]
    42 0E 00 ; Enter User Sub Map
    42 80 51 ; ADI Required Write
    42 81 51 ; ADI Required Write
    42 82 68 ; ADI Required Write
    42 03 0C ; Enable Pixel & Sync output drivers
    42 04 07 ; Power-up INTRQ pad, Enable SFL & VS pin
    42 13 00 ; Enable ADV7280A for 28_63636MHz crystal
    42 1D 40 ; Enable LLC output driver
    42 FD 84 ; Set VPP Map 
    84 A3 00 ; ADI Required Write
    84 5B 00 ; Enable Advanced Timing Mode
    84 55 80 ; Enable the Deinterlacer for I2P [All ADV7280A writes Finished]
    56 17 02 ; Reset Encoder
    56 00 9C ; Power up Encoder
    56 01 70 ; ED at 54MHz input
    56 30 1C ; 625p at 50 Hz with Embedded Timing
    56 31 01 ; Pixel Data Valid [Encoder Writes finished]
    End
    
    ##10_Program Interrupts##
    
    :Enable Analog Video Lock/Unlock Interrupts:
    42 0E 20 ; Enter Interrupt Map
    42 44 03 ; Unmask SD_LOCK and SD_UNLOCK interrupts
    42 43 03 ; Clear Clear SD_LOCK and SD_UNLOCK interrupts
    42 40 D1 ; Set INTRQ pin to drive low when active and remain low until cleared
    42 0E 00 ; Enter User Map
    End
    
    :Clear Analog Video Lock/Unlock Interrupts:
    42 0E 20 ; Enter Interrupt Map
    42 43 03 ; Clear Clear SD_LOCK and SD_UNLOCK interrupts
    42 0E 00 ; Enter User Map
    End

    Hi All,
    We have verified this behavior in our test bench using the attached script. All the scripts generate the proper video. Kindly verify your settings with this script and let us know the results

    Thanks,
    Ebin

  • Hi Ebin,

    Thank you for the scripts.

    We solved the issue by changing the ADV7280A VBI-to-active-line controls:

    42 EB 05
    42 EC 05

    Previously we had:

    42 EB 55
    42 EC 55

    With 0xEB = 0x05 and 0xEC = 0x05, the unstable chroma artifacts on the first active NTSC line disappear. The output remains in BT.656-4 mode.

    Our understanding is that these registers control when comb filtering and color output start after VBI, and our STANAG Class C / NTSC source required this to start one line earlier.

    Best regards,
    Jonathan

Reply
  • Hi Ebin,

    Thank you for the scripts.

    We solved the issue by changing the ADV7280A VBI-to-active-line controls:

    42 EB 05
    42 EC 05

    Previously we had:

    42 EB 55
    42 EC 55

    With 0xEB = 0x05 and 0xEC = 0x05, the unstable chroma artifacts on the first active NTSC line disappear. The output remains in BT.656-4 mode.

    Our understanding is that these registers control when comb filtering and color output start after VBI, and our STANAG Class C / NTSC source required this to start one line earlier.

    Best regards,
    Jonathan

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.