ADV7403
Production
The ADV7403 is a high quality, single chip, multiformat video decoder and graphics digitizer. This multiformat decoder supports the conversion of PAL,...
Datasheet
ADV7403 on Analog.com
I am decoding an NTSC CVBS signal with the ADV7403, the registers are configured with the values in Table 126 in ADV7403_Manual_RevB.
The output is YCrCB 422.
What changes do I need to make to the registers to have a RGB 444 output?
Do you have a table that defines all the register settings for CVBS in & RGB out?
Thanks
Jeff
Hi,
Please refer to Table 8 for INSEL[3:0] (Input Selection) at Address 0x00 [3:0], and Table 12 for PRIM_MODE[3:0] (Primary Mode Selection) at Address 0x05 [3:0] and VID_STD[3:0] (Video Standard Selection) at Address 0x06 [3:0] in ADV7403_Manual_RevB.
Thanks,
Ebin
Hi,
Please refer to Table 8 for INSEL[3:0] (Input Selection) at Address 0x00 [3:0], and Table 12 for PRIM_MODE[3:0] (Primary Mode Selection) at Address 0x05 [3:0] and VID_STD[3:0] (Video Standard Selection) at Address 0x06 [3:0] in ADV7403_Manual_RevB.
Thanks,
Ebin