Post Go back to editing

End-to-End Latency of ADV7613 (HDMI Input to LVDS Output

Thread Summary

The user inquires about the typical end-to-end latency of the ADV7613 from HDMI input to LVDS output. The engineer specifies that the maximum video path latency is 50 pixel clocks, and for 1080p 60Hz (148.5MHz), this translates to 336ns. The audio path latency is 70 audio sample clocks.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV7613

Does anyone know the typical end-to-end latency of the ADV7613, from HDMI input to LVDS output?

Any references to datasheets, application notes, or real-world measurements would be appreciated.

Parents
  • Hi,
         Latency is dependent on the format and what processing is being done on the stream. If you vary the format the latency also varied.  In general the image delay will always be much less then one line length measured in pixel clocks.
       
        The maximum latency of the Video path for ADV761x : 50 pixel clocks.
        The maximum latency of the Audio path for ADV761x : 70 audio sample clocks.

     For example, assuming video is 1080p 60Hz (148.5MHz) 
        Latency for 1920x1080p -- 40-50 pixel clocks
        ADV761x Video 50 pixel clocks => 148.5MHz (6.73ns) x 50 = 336ns
         
    Thanks,
    Ebin

Reply Children
No Data