Does anyone know the typical end-to-end latency of the ADV7613, from HDMI input to LVDS output?
Any references to datasheets, application notes, or real-world measurements would be appreciated.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADV7613
Recommended for New Designs
The ADV7613 is a high quality, low power, single-input HDMI
to LVDS display bridge. It incorporates an HDMI capable
receiver that supports up to 1080p...
Datasheet
ADV7613 on Analog.com
Does anyone know the typical end-to-end latency of the ADV7613, from HDMI input to LVDS output?
Any references to datasheets, application notes, or real-world measurements would be appreciated.
Hi,
Latency is dependent on the format and what processing is being done on the stream. If you vary the format the latency also varied. In general the image delay will always be much less then one line length measured in pixel clocks.
The maximum latency of the Video path for ADV761x : 50 pixel clocks.
The maximum latency of the Audio path for ADV761x : 70 audio sample clocks.
For example, assuming video is 1080p 60Hz (148.5MHz)
Latency for 1920x1080p -- 40-50 pixel clocks
ADV761x Video 50 pixel clocks => 148.5MHz (6.73ns) x 50 = 336ns
Thanks,
Ebin
Thanks a lot