Post Go back to editing

Query on Black bands seen with ADV7281

Thread Summary

The user is experiencing black bands in the video output from the ADV7281 when configured for BT.656-3 480i, even though the source video does not have these bands. The final answer suggests cropping the extra black lines on the vertical and horizontal dimensions at the SoC level, starting processing at line 23 and stopping 5 lines before the frame end, and cropping 720 to 704 on the horizontal dimension. The ADV7281 is working within the standards, and any black region must be compensated for within the SoC.
AI Generated Content
Category: Hardware
Product Number: ADV7281A

Currently we are using ADV7281A in our design where we have a source which is sending 720x480i input to the ADV7281A.

We have configured ADV7281A to output BT.656-3 480i, And, we are receiving 720x253 (even field) and 720x254 (odd field) at the SOC CSI RX.

 After deinterlacing, we see that the deinterlaced 720x507 frame has horizontal and vertical black bands at the bottom, top and right side of the image. As shown in the pic below:

We have verified that the 720x253 (even field) and 720x254 (odd field) received by the SOC have the black bands and its not due to the deinterlacing.
Our source does not have any black bands in the input video stream.

 Additionally, we also see a horizontal black line on the right side.

From the user guide we see that ADV7281A can only output either BT.656-3 or BT.656-4 complaint video.

Based on this observation we have following questions to you

  1. Can you confirm that ADV7281A is introducing the black bands at the top and bottom to be complaint to BT.656-3?
  2. How can we get rid of the horizontal black bands at the top and bottom?
    1. If we cannot avoid, can we move the black band to the bottom?
  3. How can we get rid of the vertical black band on the right side completely?

 The pic shows the number of black lines for you reference (highlighted with neon color), based on the number of lines can you share the register settings to get rid of both horizontal and vertical the black lines?

Parents
  • Hi,

     By default, the ADV728x will output in 'ITU BT656-3' timing format .If the receiver chip is expecting 'ITU BT656-4' format then this can result in 10 more dark lines appearing at the top of the screen in NTSC mode. 

    This is because 'ITU BT656-3' format has 10 more lines of vertical blanking than 'ITU BT656-4' format. 

    Also if you have not tried '0x04[7]' bit, then program the ADV728x to output in 'ITU BT656-4' format (Set User Map, register 0x04 bit[7] to 1).

    Kindly check ADV728x hardware manual for more information: http://www.analog.com/media/en/technical-documentation/user-guides/ADV7280_7281_7282_7283_UG-637.pdf

    Thanks,

    Poornima

  • Hello Poornima,

    Thank you for the quick response.

    Yes, we have already attempted the above suggestion in parallel setting register 0x04 bit[7] to 1. This adjustment has helped reduce the number of black lines at the top from 22 to 2. However, the black lines at the bottom and on the right side remain unchanged.

    Additionally, we have the following queries:

    1) How can we eliminate the horizontal black bands at the top and bottom?
      a. If removal is not possible, is there a way to shift the black band entirely to the bottom?
    2) How can we completely remove the vertical black band on the right side?

  • Hi,

      Please try with HS/VS position control registers for image shipment and for more details refer Page '77,78' at https://www.analog.com/media/en/technical-documentation/user-guides/adv7280_7281_7282_7283_ug-637.pdf

    Also, Please make sure with crystal clock (i.e) Make sure you are providing correct XTAL 28.6363.

    Thanks,

    Poornima

  • Hello,

    Please find the response in-line:

      Please try with HS/VS position control registers for image shipment and for more details refer Page '77,78' at https://www.analog.com/media/en/technical-documentation/user-guides/adv7280_7281_7282_7283_ug-637.pdf

    The current values of the HS Position Control registers are as follows:

    Reg 0x34 = 0x00
    Reg 0x35 = 0x02
    Reg 0x36 = 0x00
    To shift the image 4 pixels to the RIGHT (to eliminate the black 4 pixels on the right side):

    HSB_new = 2 + 4 = 6 → 0x006
    HSE_new = 0 + 4 = 4 → 0x004
    Updated register values:

    Reg 0x34 = 0x00
    Reg 0x35 = 0x06
    Reg 0x36 = 0x04
    However, modifying these registers did not result in any visible change in the video output.
    According to the datasheet, the HS Position Control registers are used to configure the output HSYNC. The ADV7281 variant being used does not include Sync Output Pins, which might explain the lack of effect.

    Do we have any other options to eliminate the black lines ?

    Also, Please make sure with crystal clock (i.e) Make sure you are providing correct XTAL 28.6363.

    Yes, 28,63636MHz crystal is connected.

  • Hi,

      I believe the camera is trying to generate some sort of "Letter Box" format so that might be the reason for black band/lines.

      Please try configuring 'letterbox' related registers at  https://www.analog.com/media/en/technical-documentation/user-guides/adv7280_7281_7282_7283_ug-637.pdf

      Also kindly refer here  ADV7181C Letterbox detection issue 

    Thanks,

    Poornima

  • Hello Poornima,

    Thanks for the reply. PFB the response in-line:

    Reg 0x34 = 0x00
    Reg 0x35 = 0x06
    Reg 0x36 = 0x04
    However, modifying these registers did not result in any visible change in the video output.
    According to the datasheet, the HS Position Control registers are used to configure the output HSYNC. The ADV7281 variant being used does not include Sync Output Pins, which might explain the lack of effect.

    Do we have any other options to eliminate the black lines ?

    Is this assumption correct? Can we confirm whether the HS Position Control registers only affect the Sync Output Pins (if available) or will they also modify the embedded video stream HS timing?

      I believe the camera is trying to generate some sort of "Letter Box" format so that might be the reason for black band/lines.

    We have already connected the camera unit's output to an analog NTSC monitor, which displays the video stream without any black lines. According to the camera specifications, it outputs a 480i stream, suggesting that the black bars are not introduced by the video source.

      Please try configuring 'letterbox' related registers at  https://www.analog.com/media/en/technical-documentation/user-guides/adv7280_7281_7282_7283_ug-637.pdf

      Also kindly refer here  ADV7181C Letterbox detection issue 

    Attached is the complete user sub-map register dump of the ADV7281 for the video streaming use case. The observed values for the letterbox data registers are as follows:


    addr 0x0 data 0xe
    addr 0x1 data 0xc8
    addr 0x2 data 0x44
    addr 0x3 data 0x4e
    addr 0x4 data 0x57
    addr 0x5 data 0x0
    addr 0x6 data 0x2
    addr 0x7 data 0x7f
    addr 0x8 data 0x80
    addr 0x9 data 0x80
    addr 0xa data 0x0
    addr 0xb data 0x0
    addr 0xc data 0x36
    addr 0xd data 0x7c
    addr 0xe data 0x20
    addr 0xf data 0x0
    addr 0x10 data 0x5
    addr 0x11 data 0x43
    addr 0x12 data 0x0
    addr 0x13 data 0x69
    addr 0x14 data 0x10
    addr 0x15 data 0x8
    addr 0x16 data 0x40
    addr 0x17 data 0x41
    addr 0x18 data 0x93
    addr 0x19 data 0xf1
    addr 0x1a data 0x58
    addr 0x1b data 0x1
    addr 0x1c data 0xab
    addr 0x1d data 0xc0
    addr 0x1e data 0x16
    addr 0x1f data 0x10
    addr 0x20 data 0xe2
    addr 0x21 data 0x51
    addr 0x22 data 0x4b
    addr 0x23 data 0xc4
    addr 0x24 data 0x5
    addr 0x25 data 0x0
    addr 0x26 data 0x22
    addr 0x27 data 0x58
    addr 0x28 data 0xc
    addr 0x29 data 0x38
    addr 0x2a data 0x20
    addr 0x2b data 0xe1
    addr 0x2c data 0xae
    addr 0x2d data 0xf5
    addr 0x2e data 0xae
    addr 0x2f data 0xf6
    addr 0x30 data 0xf4
    addr 0x31 data 0x2
    addr 0x32 data 0x41
    addr 0x33 data 0x84
    addr 0x34 data 0x0
    addr 0x35 data 0x2
    addr 0x36 data 0x0
    addr 0x37 data 0x81
    addr 0x38 data 0x80
    addr 0x39 data 0xc0
    addr 0x3a data 0x0
    addr 0x3b data 0x44
    addr 0x3c data 0x58
    addr 0x3d data 0x22
    addr 0x3e data 0x64
    addr 0x3f data 0xe4
    addr 0x40 data 0x18
    addr 0x41 data 0x0
    addr 0x42 data 0x0
    addr 0x43 data 0x0
    addr 0x44 data 0x0
    addr 0x45 data 0x0
    addr 0x46 data 0x0
    addr 0x47 data 0x0
    addr 0x48 data 0x0
    addr 0x49 data 0x6
    addr 0x4a data 0x0
    addr 0x4b data 0x0
    addr 0x4c data 0x80
    addr 0x4d data 0x0
    addr 0x4e data 0x0
    addr 0x4f data 0x0
    addr 0x50 data 0x8
    addr 0x51 data 0x20
    addr 0x52 data 0x0
    addr 0x53 data 0x0
    addr 0x54 data 0x0
    addr 0x55 data 0x0
    addr 0x56 data 0x0
    addr 0x57 data 0x0
    addr 0x58 data 0x0
    addr 0x59 data 0x0
    addr 0x5a data 0x0
    addr 0x5b data 0x0
    addr 0x5c data 0x0
    addr 0x5d data 0x0
    addr 0x5e data 0x0
    addr 0x5f data 0x0
    addr 0x60 data 0x88
    addr 0x61 data 0x10
    addr 0x62 data 0x15
    addr 0x63 data 0x6e
    addr 0x64 data 0x0
    addr 0x65 data 0x0
    addr 0x66 data 0x0
    addr 0x67 data 0x0
    addr 0x68 data 0x0
    addr 0x69 data 0x0
    addr 0x6a data 0x0
    addr 0x6b data 0x0
    addr 0x6c data 0x0
    addr 0x6d data 0x0
    addr 0x6e data 0x0
    addr 0x6f data 0x0
    addr 0x70 data 0x0
    addr 0x71 data 0x0
    addr 0x72 data 0x0
    addr 0x73 data 0x0
    addr 0x74 data 0x0
    addr 0x75 data 0x0
    addr 0x76 data 0x0
    addr 0x77 data 0x0
    addr 0x78 data 0x0
    addr 0x79 data 0x0
    addr 0x7a data 0x0
    addr 0x7b data 0x0
    addr 0x7c data 0x0
    addr 0x7d data 0x0
    addr 0x7e data 0x0
    addr 0x7f data 0x0
    addr 0x80 data 0x0
    addr 0x81 data 0x0
    addr 0x82 data 0x0
    addr 0x83 data 0x0
    addr 0x84 data 0x0
    addr 0x85 data 0x0
    addr 0x86 data 0x0
    addr 0x87 data 0x0
    addr 0x88 data 0x0
    addr 0x89 data 0x0
    addr 0x8a data 0x0
    addr 0x8b data 0x0
    addr 0x8c data 0x0
    addr 0x8d data 0x0
    addr 0x8e data 0x0
    addr 0x8f data 0x0
    addr 0x90 data 0x0
    addr 0x91 data 0x0
    addr 0x92 data 0x0
    addr 0x93 data 0x0
    addr 0x94 data 0x0
    addr 0x95 data 0x0
    addr 0x96 data 0x0
    addr 0x97 data 0x0
    addr 0x98 data 0x0
    addr 0x99 data 0x0
    addr 0x9a data 0x0
    addr 0x9b data 0x0
    addr 0x9c data 0x30
    addr 0x9d data 0x0
    addr 0x9e data 0x0
    addr 0x9f data 0x0
    addr 0xa0 data 0x0
    addr 0xa1 data 0x0
    addr 0xa2 data 0x0
    addr 0xa3 data 0x0
    addr 0xa4 data 0x0
    addr 0xa5 data 0x0
    addr 0xa6 data 0x0
    addr 0xa7 data 0x0
    addr 0xa8 data 0x0
    addr 0xa9 data 0x0
    addr 0xaa data 0x0
    addr 0xab data 0x0
    addr 0xac data 0x0
    addr 0xad data 0x0
    addr 0xae data 0x0
    addr 0xaf data 0x0
    addr 0xb0 data 0x0
    addr 0xb1 data 0x0
    addr 0xb2 data 0x0
    addr 0xb3 data 0x0
    addr 0xb4 data 0x0
    addr 0xb5 data 0x0
    addr 0xb6 data 0x0
    addr 0xb7 data 0x0
    addr 0xb8 data 0x0
    addr 0xb9 data 0x0
    addr 0xba data 0x0
    addr 0xbb data 0x0
    addr 0xbc data 0x0
    addr 0xbd data 0x0
    addr 0xbe data 0x0
    addr 0xbf data 0x0
    addr 0xc0 data 0x0
    addr 0xc1 data 0x0
    addr 0xc2 data 0x0
    addr 0xc3 data 0x0
    addr 0xc4 data 0x0
    addr 0xc5 data 0x0
    addr 0xc6 data 0x0
    addr 0xc7 data 0x0
    addr 0xc8 data 0x0
    addr 0xc9 data 0x0
    addr 0xca data 0x0
    addr 0xcb data 0x0
    addr 0xcc data 0x0
    addr 0xcd data 0x0
    addr 0xce data 0x0
    addr 0xcf data 0x0
    addr 0xd0 data 0x0
    addr 0xd1 data 0x0
    addr 0xd2 data 0x0
    addr 0xd3 data 0x0
    addr 0xd4 data 0x0
    addr 0xd5 data 0x0
    addr 0xd6 data 0x0
    addr 0xd7 data 0x0
    addr 0xd8 data 0x0
    addr 0xd9 data 0x0
    addr 0xda data 0x0
    addr 0xdb data 0x0
    addr 0xdc data 0x0
    addr 0xdd data 0x0
    addr 0xde data 0x0
    addr 0xdf data 0x0
    addr 0xe0 data 0x0
    addr 0xe1 data 0x0
    addr 0xe2 data 0x0
    addr 0xe3 data 0x0
    addr 0xe4 data 0x0
    addr 0xe5 data 0x0
    addr 0xe6 data 0x0
    addr 0xe7 data 0x0
    addr 0xe8 data 0x0
    addr 0xe9 data 0x0
    addr 0xea data 0x0
    addr 0xeb data 0x0
    addr 0xec data 0x0
    addr 0xed data 0x0
    addr 0xee data 0x0
    addr 0xef data 0x0
    addr 0xf0 data 0x0
    addr 0xf1 data 0x0
    addr 0xf2 data 0x0
    addr 0xf3 data 0x0
    addr 0xf4 data 0x0
    addr 0xf5 data 0x0
    addr 0xf6 data 0x0
    addr 0xf7 data 0x0
    addr 0xf8 data 0x0
    addr 0xf9 data 0x0
    addr 0xfa data 0x0
    addr 0xfb data 0x0
    addr 0xfc data 0x0
    addr 0xfd data 0x0
    addr 0xfe data 0x0
    addr 0xff data 0x0

    - LB_LCT (0x9B): 0x0  
    - LB_LCM (0x9C): 0x30  
    - LB_LCB (0x9D): 0x0  

    Attempts to modify the Letterbox Control registers were made, but after successfully writing to the 0xDC and 0xDD registers, the values were not retained, as subsequent reads of the registers returned 0x00.

    From the hardware manual, it appears that the letterbox feature only detects black lines in the incoming video. Can it also remove the black lines in the ADV7281 video output?

  • Hi,

      From the hardware manual, it appears that the letterbox feature only detects black lines in the incoming video. Can it also remove the black lines in the ADV7281 video output ?

        Yes, letterbox feature detects only black lines in the incoming video but it will not remove or add any black lines in the ADV728x output (It just passthrough the video).

     Also Please let us know, Have you verified the same issue with back to back connection/Direct Connection ( Source --> Sink) ?

    Thanks,

    Poornima

  • Hello Poornima,

    I'm the team mate of the author.

    We have verified the source by directly connecting it to a monitor (No ADV7281 involved). No black lines seen vertical or horizontal.

     

    Its clear that ADV7281 is inserting the horizontal black line to be complaint to ITU-BT656 standard.

    Our customer wants the horizontal black lines removed or make it symmetric.

     

    In additional we still dint understand why the vertical black like is inserted by ADV7281.

    Please support us!

Reply
  • Hello Poornima,

    I'm the team mate of the author.

    We have verified the source by directly connecting it to a monitor (No ADV7281 involved). No black lines seen vertical or horizontal.

     

    Its clear that ADV7281 is inserting the horizontal black line to be complaint to ITU-BT656 standard.

    Our customer wants the horizontal black lines removed or make it symmetric.

     

    In additional we still dint understand why the vertical black like is inserted by ADV7281.

    Please support us!

Children
  • Hi ,

        Could you please provide the detailed setup information?

    Thanks,

    Ebin

  • Hello Ebin

    Thanks for the reply.

    Currently we are using this External Monitor which is connected to the DVR Module

    https://www.amazon.co.jp/Antion-4-3%E3%82%A4%E3%83%B3%E3%83%81%E3%83%A2%E3%83%8B%E3%82%BF%E3%83%BC-…

     

    Thank You

    Akash

  • Hi Akash,

        Thanks for the information. Could you please check the video output by enable the free run option in 0x0c[0] and let us know the status?

    Thanks,
    Ebin

  • Hello Ebin,

    We are not observing any black bands in the free run mode.
    Used 0x0C[bit 0](DEF_VAL_EN) = 1 to force free-run mode on and could observe the default solid blue frame without any black borders

  • Hi Rajendraprasad,

    Thank you for your response. Please let us know the status of the output with the following configuration checks:

    1. Please try using a different source.
    2. Ensure that during power-up, the reset pin is held low for at least 5 ms after the 3.3 V, 1.8 V, and power-down lines go high. After the reset pin goes high, wait at least 5 ms before starting I2C communication.
    3. Try toggling the polarity bit in register 0x37 to see if the edge issue disappears, and also modify registers 0xE5 to 0xEA.
    4. Write 0x00 to User Sub Map 2, register 0x84.

    Thanks,
    Ebin

  • Hi  Ebin 

    1. Please try using a different source.

    we are not able to verify with other source as we don't have any other source with compatible connector

    2. Ensure that during power-up, the reset pin is held low for at least 5 ms after the 3.3 V, 1.8 V, and power-down lines go high. After the reset pin goes high, wait at least 5 ms before starting I2C communication.

    We have verified that during power-up, the reset pin is held low for at least 5 ms after the 3.3 V, 1.8 V, and PWRDN lines go high.
    After the reset pin is released, we also wait an additional 5 ms before initiating any I²C communication.

     

    3. Try toggling the polarity bit in register 0x37 to see if the edge issue disappears, and also modify registers 0xE5 to 0xEA.

    We tried toggling the different combinations of polarity bit in register 0x37, but the black bars are still present.

    PHS (7)

    PVS (5)

    PF (3)

    PCLK (0)

    Binary (bit7→bit0)

    HEX

    0

    0

    0

    0

    0000 0000

    0x00

    0

    0

    0

    1

    0000 0001

    0x01

    0

    0

    1

    0

    0000 1000

    0x08

    0

    0

    1

    1

    0000 1001

    0x09

    0

    1

    0

    0

    0010 0000

    0x20

    0

    1

    0

    1

    0010 0001

    0x21

    0

    1

    1

    0

    0010 1000

    0x28

    0

    1

    1

    1

    0010 1001

    0x29

    1

    0

    0

    0

    1000 0000

    0x80

    1

    0

    0

    1

    1000 0001

    0x81

    1

    0

    1

    0

    1000 1000

    0x88

    1

    0

    1

    1

    1000 1001

    0x89

    1

    1

    0

    0

    1010 0000

    0xA0

    1

    1

    0

    1

    1010 0001

    0xA1

    1

    1

    1

    0

    1010 1000

    0xA8

    1

    1

    1

    1

    1010 1001

    0xA9

    We modified the registers in the 0xE5–0xE7 range, but there was no visible change in the black band issue.

    Enable the 0X31 Register VS/FIELD Control 1 for registers 0xE5 to 0xEA

    VS/FIELD Control 1   0x31 00010010 [ 0x12 ]

    NTSC VSYNC begin   0xE5 11000101 [ 0xc5]

    NTSC VSYNC end       0xE6 11000100 [ 0xc4 ]

    NTSC FIELD toggle     0xE7 11000011 [ 0xc3 ]

     

    we didn't tried from E8 to EA because these are related to PAL Standard

     

    4. Write 0x00 to User Sub Map 2, register 0x84.

    We wrote 0x00 to register 0x84 as suggested.
    However, the black band is still observed, and the issue persists.


    Thanks,
    Akash

  • Hi Akash,

        Thanks for your confirmation .

    Can you please confirm the below points ?

        1. We understand that the output of the ADV7821 is 720×253 and 720×254 frames, which is the correct resolution for the BT.656-3 480i format. This signal is provided to the SoC, but the output on the monitor shows black bands. Please verify whether the SoC is configured correctly.
    2. In NTSC mode, the ADV728x outputs a 60 Hz refresh rate. Could you check whether your display supports 60 Hz, or is it limited to 50 Hz?

    Thanks,
    Ebin

  • Hello Ebin,

    Thanks for your response.

    We do not suspect the SoC, as we also observe the black bands when dumping the raw buffer output from the ADV7281.

    As mentioned earlier(on Nov 18, 2025 2:19 PM), modifying to ITU BT.656-4, which outputs 720×243 and 720×244 frames, reduces the number of black lines at the bottom from 22 to 2.

    Based on this, we suspect that the ADV7281 is adding black lines to the source video (480i [720x480]). Specifically:

    - Using BT.656-3, 480i after de-interlacing becomes 720x507. Here, we observe 27 horizontal black lines (22 at the top and 5 at the bottom) with a 720x480 video source (507 - 480 = 27).
    - Using BT.656-4, 480i after de-interlacing becomes 720x487. Here, we observe 7 horizontal black lines (2 at the top and 5 at the bottom) with a 720x480 video source (487 - 480 = 7).

    Additionally, we observe 5 vertical black lines on the right side, which suggests that the input video frames are cropped, resulting in data loss.

    We would like your assistance in understanding how to avoid or mitigate these black lines.

  • Hi ,
    We have suggested the following response to the customer:
       The SoC can Crop the extra black lines on the vertical dimension and Horizontal dimension. We suggested they can simply start processing at line 23 and stop 5 lines before frame end on the vertical dimensions and crop the extra black lines crop 720 to 704 on the Horizontal dimension .ADV728x is working within the boundaries of the standards, any black region is acceptable and must be compensated within the SoC.

    Customer has responded below:    
        we will crop the extra black lines from the ADV output. We have no further queries.

    Thanks,
    Ebin