Post Go back to editing

ADV7181C Register Settings for STANAG3350 Signals

Category: Hardware
Product Number: ADV7181C

Hello ADI Team,

We are using ADV7181C video decoder with STANAG3350 B inputs. With the auto detect option register settings, when we give are seeing slight jitter on the image. But if we try signals from an NTSC based signal (STANAG 3350 C), then we are not seeing the jitter.

I was trying to do manual settings for PLL RATIO, But the table 11 in the user manual does not list a recommended value for video standard which has 625 lines.

Could you please guide me?

if you can suggest the register settings for STANAG3350 B, it will be of great help.

Thanks,

Paul

Parents
  • Thank you Poornima,

    But this document is not for ADV7181C. Does it matter?

    My main question was why does Table 11 in the User Manual of ADV7181C does not list a lines per frame of 625?

    Thanks and regards,

    Paul

  • Hi,

       Yes, We can use this application note(AN-0978) for configuring the non standard mode.

       In 'Table 11' we have the PLL Recommended settings for 625 total lines (Lines per frame 625 total lines (576 Active lines)). Please check

    Thanks,

    Poornima

  • Hi Poornima,

    Thanks, the highlighted value in the above table is for progressive scan, right?

    Shouldn't we use one of them from last two items in the table?

    Thanks and regards,

    Paul

  • Hi,

    Shouldn't we use one of them from last two items in the table ?

      Yes, you can use the last two items; I just highlighted them for 576p.

    Thanks,

    Poornima

  • Hi Poornima,

    We tried that option also still seeing some pixel jittering/shivering mainly where white to black transition is there and the frequency of vibration is varying with two frequencies at the order of a few Hz. Faster frequency for about 10s and other frequency for about 6 seconds.

    As mentioned this is visible at the boundaries where contrast is there. Will you be able to throw some lights here?

    Strangely, this is observed only for PAL signals and not observed (or not that much visible) for NTSC based signals.

    Thanks and regards,

    Paul 

  • Hi,

     Instead of autodetect, Please force the specific video standard according to the below 'VID_SEL' configuration,

     Also If possible, kindly share your register configuration.

    Thanks,

    Poornima

  • Hi Poornima,

    Below are the register settings we use.

    Thanks and regards,

    Paul


    Address: 0x0 Data: 0x0 Address: 0x1 Data: 0xC8 Address: 0x2 Data: 0x4 Address: 0x3 Data: 0xC Address: 0x4 Data: 0x75 Address: 0x5 Data: 0x0 Address: 0x6 Data: 0xB Address: 0x7 Data: 0x7F Address: 0x8 Data: 0x80 Address: 0x9 Data: 0x80 Address: 0xA Data: 0x0 Address: 0xB Data: 0x0 Address: 0xC Data: 0x10 Address: 0xD Data: 0x88 Address: 0xE Data: 0x0 Address: 0xF Data: 0x0 Address: 0x10 Data: 0x4B Address: 0x11 Data: 0x19 Address: 0x12 Data: 0x80 Address: 0x13 Data: 0xC Address: 0x14 Data: 0x12 Address: 0x15 Data: 0x8 Address: 0x16 Data: 0x11 Address: 0x17 Data: 0x1 Address: 0x18 Data: 0x93 Address: 0x19 Data: 0xF1 Address: 0x1A Data: 0x40 Address: 0x1B Data: 0x3 Address: 0x1C Data: 0x4 Address: 0x1D Data: 0x47 Address: 0x1E Data: 0x82 Address: 0x1F Data: 0x15 Address: 0x20 Data: 0x88 Address: 0x21 Data: 0x20 Address: 0x22 Data: 0x80 Address: 0x23 Data: 0xCB Address: 0x24 Data: 0x64 Address: 0x25 Data: 0x11 Address: 0x26 Data: 0xD1 Address: 0x27 Data: 0x58 Address: 0x28 Data: 0x5 Address: 0x29 Data: 0xB4 Address: 0x2A Data: 0x9E Address: 0x2B Data: 0xE1 Address: 0x2C Data: 0xAE Address: 0x2D Data: 0xF2 Address: 0x2E Data: 0x64 Address: 0x2F Data: 0xF4 Address: 0x30 Data: 0xC9 Address: 0x31 Data: 0x12 Address: 0x32 Data: 0x41 Address: 0x33 Data: 0x84 Address: 0x34 Data: 0x0 Address: 0x35 Data: 0x2 Address: 0x36 Data: 0x0 Address: 0x37 Data: 0x1 Address: 0x38 Data: 0x80 Address: 0x39 Data: 0xC0 Address: 0x3A Data: 0x11 Address: 0x3B Data: 0x81 Address: 0x3C Data: 0x52 Address: 0x3D Data: 0x43 Address: 0x3E Data: 0x50 Address: 0x3F Data: 0xE0 Address: 0x40 Data: 0x90 Address: 0x41 Data: 0x1 Address: 0x42 Data: 0x7E Address: 0x43 Data: 0xA4 Address: 0x44 Data: 0xFF Address: 0x45 Data: 0xB6 Address: 0x46 Data: 0x12 Address: 0x47 Data: 0xFF Address: 0x48 Data: 0x0 Address: 0x49 Data: 0x0 Address: 0x4A Data: 0x0 Address: 0x4B Data: 0x0 Address: 0x4C Data: 0x0 Address: 0x4D Data: 0xEF Address: 0x4E Data: 0x8 Address: 0x4F Data: 0x8 Address: 0x50 Data: 0x8 Address: 0x51 Data: 0x24 Address: 0x52 Data: 0x0 Address: 0x53 Data: 0x0 Address: 0x54 Data: 0x12 Address: 0x55 Data: 0x90 Address: 0x56 Data: 0x38 Address: 0x57 Data: 0x69 Address: 0x58 Data: 0x48 Address: 0x59 Data: 0x8 Address: 0x5A Data: 0x0 Address: 0x5B Data: 0x75 Address: 0x5C Data: 0x21 Address: 0x5D Data: 0x0 Address: 0x5E Data: 0x1A Address: 0x5F Data: 0xB8 Address: 0x60 Data: 0x8 Address: 0x61 Data: 0x0 Address: 0x62 Data: 0x20 Address: 0x63 Data: 0x3 Address: 0x64 Data: 0xD7 Address: 0x65 Data: 0x19 Address: 0x66 Data: 0x48 Address: 0x67 Data: 0x13 Address: 0x68 Data: 0x1 Address: 0x69 Data: 0x0 Address: 0x6A Data: 0x0 Address: 0x6B Data: 0x1 Address: 0x6C Data: 0x0 Address: 0x6D Data: 0x0 Address: 0x6E Data: 0x0 Address: 0x6F Data: 0x0 Address: 0x70 Data: 0x0 Address: 0x71 Data: 0x0 Address: 0x72 Data: 0x0 Address: 0x73 Data: 0xCF Address: 0x74 Data: 0xA3 Address: 0x75 Data: 0xE8 Address: 0x76 Data: 0xFA Address: 0x77 Data: 0x3F Address: 0x78 Data: 0xFF Address: 0x79 Data: 0xFF Address: 0x7A Data: 0xFF Address: 0x7B Data: 0x6 Address: 0x7C Data: 0xC0 Address: 0x7D Data: 0x0 Address: 0x7E Data: 0x0 Address: 0x7F Data: 0x0 Address: 0x80 Data: 0x0 Address: 0x81 Data: 0xD0 Address: 0x82 Data: 0x4 Address: 0x83 Data: 0x0 Address: 0x84 Data: 0xC Address: 0x85 Data: 0x19 Address: 0x86 Data: 0x1B Address: 0x87 Data: 0x63 Address: 0x88 Data: 0x5A Address: 0x89 Data: 0x8 Address: 0x8A Data: 0x10 Address: 0x8B Data: 0x4 Address: 0x8C Data: 0x41 Address: 0x8D Data: 0x0 Address: 0x8E Data: 0x4E Address: 0x8F Data: 0x0 Address: 0x90 Data: 0x0 Address: 0x91 Data: 0x0 Address: 0x92 Data: 0x0 Address: 0x93 Data: 0x0 Address: 0x94 Data: 0x0 Address: 0x95 Data: 0x0 Address: 0x96 Data: 0x0 Address: 0x97 Data: 0x0 Address: 0x98 Data: 0x0 Address: 0x99 Data: 0x0 Address: 0x9A Data: 0x0 Address: 0x9B Data: 0x0 Address: 0x9C Data: 0x0 Address: 0x9D Data: 0x0 Address: 0x9E Data: 0x96 Address: 0x9F Data: 0x11 Address: 0xA0 Data: 0x3 Address: 0xA1 Data: 0xFF Address: 0xA2 Data: 0x1 Address: 0xA3 Data: 0x1C Address: 0xA4 Data: 0x1D Address: 0xA5 Data: 0x1C Address: 0xA6 Data: 0x88 Address: 0xA7 Data: 0x3C Address: 0xA8 Data: 0xF5 Address: 0xA9 Data: 0xFF Address: 0xAA Data: 0xFF Address: 0xAB Data: 0xF Address: 0xAC Data: 0x88 Address: 0xAD Data: 0x0 Address: 0xAE Data: 0x39 Address: 0xAF Data: 0xB Address: 0xB0 Data: 0xD Address: 0xB1 Data: 0xF9 Address: 0xB2 Data: 0x3E Address: 0xB3 Data: 0x21 Address: 0xB4 Data: 0x3C Address: 0xB5 Data: 0x7 Address: 0xB6 Data: 0x0 Address: 0xB7 Data: 0x0 Address: 0xB8 Data: 0x40 Address: 0xB9 Data: 0x0 Address: 0xBA Data: 0x0 Address: 0xBB Data: 0x1 Address: 0xBC Data: 0x5C Address: 0xBD Data: 0x0 Address: 0xBE Data: 0xA0 Address: 0xBF Data: 0x6 Address: 0xC0 Data: 0x10 Address: 0xC1 Data: 0x80 Address: 0xC2 Data: 0x80 Address: 0xC3 Data: 0x46 Address: 0xC4 Data: 0x85 Address: 0xC5 Data: 0x1 Address: 0xC6 Data: 0x0 Address: 0xC7 Data: 0x0 Address: 0xC8 Data: 0x0 Address: 0xC9 Data: 0xC Address: 0xCA Data: 0x8 Address: 0xCB Data: 0xB9 Address: 0xCC Data: 0x5B Address: 0xCD Data: 0x0 Address: 0xCE Data: 0x1 Address: 0xCF Data: 0xB4 Address: 0xD0 Data: 0x0 Address: 0xD1 Data: 0x10 Address: 0xD2 Data: 0xFF Address: 0xD3 Data: 0xFF Address: 0xD4 Data: 0x7F Address: 0xD5 Data: 0x7F Address: 0xD6 Data: 0x3E Address: 0xD7 Data: 0x8 Address: 0xD8 Data: 0x3C Address: 0xD9 Data: 0x8 Address: 0xDA Data: 0x3C Address: 0xDB Data: 0x9B Address: 0xDC Data: 0xAC Address: 0xDD Data: 0x4C Address: 0xDE Data: 0x0 Address: 0xDF Data: 0x0 Address: 0xE0 Data: 0x14 Address: 0xE1 Data: 0x80 Address: 0xE2 Data: 0x80 Address: 0xE3 Data: 0x80 Address: 0xE4 Data: 0x80 Address: 0xE5 Data: 0x25 Address: 0xE6 Data: 0x4 Address: 0xE7 Data: 0x63 Address: 0xE8 Data: 0x65 Address: 0xE9 Data: 0x14 Address: 0xEA Data: 0x63 Address: 0xEB Data: 0x55 Address: 0xEC Data: 0x55 Address: 0xED Data: 0x0 Address: 0xEE Data: 0x0 Address: 0xEF Data: 0x4A Address: 0xF0 Data: 0x44 Address: 0xF1 Data: 0x0 Address: 0xF2 Data: 0x32 Address: 0xF3 Data: 0x7 Address: 0xF4 Data: 0x55 Address: 0xF5 Data: 0xE0 Address: 0xF6 Data: 0x69 Address: 0xF7 Data: 0x10 Address: 0xF8 Data: 0x0 Address: 0xF9 Data: 0x0 Address: 0xFA Data: 0xA0 Address: 0xFB Data: 0x40 Address: 0xFC Data: 0x4
  • Hi,

      Kindly note that, Some of the above shared configurations seem to be different form our reference one So Please cross-check your configuration against our reference script - '##CP 625i##' at ez.analog.com/.../5355.ADV7181C_5F00_Evaluation_5F00_Software.zip

    Thanks,

    Poornima 

  • Hi Poornima,

    Thank you for sharing it.

    Could you please be more specific about the file. I was not able to open the .set files.

    Does the text file included in the ZIP file has this register details? It has many settings.

    I am confused about the very first register itself.

    Reg 0x00, INPUT CONTROL register, what we should select for STANAG 3350 B signals. Even though it follows PAL based timings, it is actually Component Video right? Then how should we select the CVBS composite input?

    Thanks and regards,

    Paul

  • Hi Poornima,

    We tried the below register settings (from the Script files you shared)

    ##CP YPrPb 525i & 625i##
    :625I YPrPb In 10Bit 422 Encoder:
    42 05 00 ; Prim_Mode =000b for SD-M
    42 06 0B ; VID_STD=1010b for SD 4x1 525i
    42 1D 47 ; Enable 28MHz Crystal
    42 3A 11 ; Set Latch Clock 01b, Power Down ADC3
    42 3B 81 ; Enable internal Bias
    42 3C 52 ; PLL_QPUMP to 010b
    42 6B C1 ; Select 422 10 bit YPrPb out from CP
    42 7B 06 ; clears the bits CP_DUP_AV and AV_Blank_EN
    42 85 19 ; Turn off SSPD and force SOY. For Eval Board.
    42 86 1B ; Enable stdi_line_count_mode
    42 8A B0 ; Manual VCO_RANGE=01
    42 8F 77 ; FR_LL to 1820 & Enable 28.63MHz LLC
    42 90 1C ; FR_LL to 1820
    42 BF 06 ; Blue Screen Free Run Colour
    42 C0 40 ; default color
    42 C1 F0 ; default color
    42 C2 80 ; Default color
    42 C5 01 ; CP_CLAMP_AVG_FACTOR[1-0] = 00b
    42 C9 0C ; Enable DDR Mode
    42 F3 07 ; Enable Anti Alias Filters on ADC 0,1,2
    42 0E 80 ; ADI Recommended Setting
    42 52 46 ; ADI Recommended Setting
    42 54 00 ; ADI Recommended Setting
    42 F6 3B ; ADI Recommended Setting
    42 0E 00 ; ADI Recommended Setting
    56 17 02 ; Software Reset
    56 00 FC ; Power up all DAcs and PLL
    56 01 80 ; SD only mode, Data input on Y-bus
    56 80 11 ; SSAF Luma filter enabled, NTSC mode
    56 82 C1 ; Step control on, pixel data valid, PrPb SSAF on,CVBS/YC out.
    56 84 06 ; RTCO/SFL Enable
    56 88 10 ; 10 bit input enabled
    56 87 20 ; Encoder PAL/NTSC auto-detect enabled
    End

    However, no change.

    Could you please let us know what should be the settings for 0X00. We are connecting STANAG signals to ADV7181C as follows:

    Blue - AIN4

    Red  - AIN5

    Green with Sync - AIN6

    Thanks,

    Paul

Reply
  • Hi Poornima,

    We tried the below register settings (from the Script files you shared)

    ##CP YPrPb 525i & 625i##
    :625I YPrPb In 10Bit 422 Encoder:
    42 05 00 ; Prim_Mode =000b for SD-M
    42 06 0B ; VID_STD=1010b for SD 4x1 525i
    42 1D 47 ; Enable 28MHz Crystal
    42 3A 11 ; Set Latch Clock 01b, Power Down ADC3
    42 3B 81 ; Enable internal Bias
    42 3C 52 ; PLL_QPUMP to 010b
    42 6B C1 ; Select 422 10 bit YPrPb out from CP
    42 7B 06 ; clears the bits CP_DUP_AV and AV_Blank_EN
    42 85 19 ; Turn off SSPD and force SOY. For Eval Board.
    42 86 1B ; Enable stdi_line_count_mode
    42 8A B0 ; Manual VCO_RANGE=01
    42 8F 77 ; FR_LL to 1820 & Enable 28.63MHz LLC
    42 90 1C ; FR_LL to 1820
    42 BF 06 ; Blue Screen Free Run Colour
    42 C0 40 ; default color
    42 C1 F0 ; default color
    42 C2 80 ; Default color
    42 C5 01 ; CP_CLAMP_AVG_FACTOR[1-0] = 00b
    42 C9 0C ; Enable DDR Mode
    42 F3 07 ; Enable Anti Alias Filters on ADC 0,1,2
    42 0E 80 ; ADI Recommended Setting
    42 52 46 ; ADI Recommended Setting
    42 54 00 ; ADI Recommended Setting
    42 F6 3B ; ADI Recommended Setting
    42 0E 00 ; ADI Recommended Setting
    56 17 02 ; Software Reset
    56 00 FC ; Power up all DAcs and PLL
    56 01 80 ; SD only mode, Data input on Y-bus
    56 80 11 ; SSAF Luma filter enabled, NTSC mode
    56 82 C1 ; Step control on, pixel data valid, PrPb SSAF on,CVBS/YC out.
    56 84 06 ; RTCO/SFL Enable
    56 88 10 ; 10 bit input enabled
    56 87 20 ; Encoder PAL/NTSC auto-detect enabled
    End

    However, no change.

    Could you please let us know what should be the settings for 0X00. We are connecting STANAG signals to ADV7181C as follows:

    Blue - AIN4

    Red  - AIN5

    Green with Sync - AIN6

    Thanks,

    Paul

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.