KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADV7280
Not Recommended for New Designs
The ADV7280 / ADV7280-M are versatile one-chip, multiformat video decoders. The ADV7280 / ADV7280-M automatically detect standard analog baseband video...
Datasheet
ADV7280 on Analog.com
We’re working with a custom PCB that connects a composite video camera to an ADV7280A-M and then outputs MIPI-CSI2 to a Raspberry Pi 4.
We’re using the official Raspberry Pi Linux driver:
and took inspiration from this project:
github.com/.../ADV7280-Raspi-shield
The video stream works — but with certain analog camera sources (for example, Framos CVBS modules) the image is shifted vertically:
the bottom ~20 lines of the picture wrap around and appear at the top, as shown below:

text seem to have weird colors:

With other cameras the image is perfectly aligned, so the issue might depend on the input signal timing.
Custom PCB using ADV7280A-M (8× CVBS inputs, MIPI CSI-2 output)
Connected directly to Raspberry Pi 4 Model B CSI port
Kernel: rpi-6.12.y, using stock adv7180.c driver
No modifications to driver except input selection via sub-device
Hi,
Kindly note that, By default the ADV7280 outputs according to the ITU-R BT.656-3 specification. There are extra blanking lines in the vertical blanking period for NTSC signals in ITU-R BT.656-3 mode compared to ITU-R BT.656-4 mode.
You can switch between the ITU-R BT.656-3 mode and ITU-R BT.656-4 output mode by toggling the User Map register 0x04 bit [7].
0: (default) BT656-3 mode
1: BT656-4 mode
Also make sure with crystal clock (i.e) you are providing correct 'XTAL 28.6363' and your script selects 28.63636 crystal.
Thanks,
Poornima