| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 70 hours |
Closed | |
ADV7280A
Recommended for New Designs
The ADV7280A has the same pinout as and is software compati-ble with the ADV7280. The mobile industry processor interface (MIPI®) model of the ADV7280A...
Datasheet
ADV7280A on Analog.com
Hi,
Please refer here ADV7280 / ADV7280-M Design Support Files Here you can get register configuration for NTSC and PAL standard.
Kindly note that, ADV7280x part can support standard resolutions.
Thanks,
Poornima
Hi,
Thanks for the answer but you didn't answer my question regarding the resolution support NTSC 640x480, PAL 640x480 and PAL 720x540?
BR
Shmuel
Hi,
ADV728x can support only SD -- NTSC, PAL, SECAM and their variants but it cannot take 480p, VGA, or any other custom format.
Please use I2P functionality inorder to support progressive output (480p/576p Out).
As stated in previous response, It can support only standard format so it doesn't support 720x540 resolution.
Note: ADV728x has standard definition processor (SDP) and It automatically detect standard analog baseband video signals compatible with worldwide NTSC, PAL, and SECAM standards in the form of composite, S-Video, and component video.
Please note that "I2P works by 'line-doubling' i.e. outputting the same line twice and doubling the MIPI CSI-2 clock speed".
In Interlaced mode the ADV7282-M outputs with a 216 Mbps data rate (MIPI clock frequency 108 MHz).
In Progressive mode (i.e. I2P mode Enabled) the ADV7282-M outputs a 432 Mbps data rate ( MIPI clock frequency 216 MHz).
Thanks,
Poornima
Hi,
My camera input is PAL 640x480\ NTSC 640x480\ PAL 720x540.
Does the ADV2870-M support those inputs resolutions?
BR
Shmuel
Hi ,
The ADV728x can interface with the following standard camera input formats. Please refer to the ADV728x specifications for additional details.
PAL B/G/H/I/D/N/M
PAL Combination N
PAL 60
NTSC M/J/4.43
SECAM
Please note that if the camera module outputs a custom or non-standard video format (for example, one with a non-standard line length), the ADV728x will not be able to lock onto that signal. For more information, refer to the “Output Video Format” section of the ADV728x User Guide.
Thanks,
Varshini K