Post Go back to editing

Suitability for solution? MAX96717 + MAX96716A -> MIPI-CSI, SPI, I2C

Thread Summary

The user is evaluating the MAX96717 + MAX96716A for replacing flat cables between an ARM SoC and remote imaging and sensing units, including 2x SPI IMUs with high data rates (20 bytes per reading, 1kHz to 8kHz ODR) and 2x I2C compasses. The final answer directs the user to visit the technical support pages on the Analog Devices website for further assistance, ensuring that the specific use case can be evaluated by a support engineer.
AI Generated Content
Category: Hardware
Product Number: MAX96716A , MAX967, MAX967

I am evaluating the pair of MAX96717 + MAX96716A to replace a series of flat cables between an ARM SoC and a remote imaging and sensing units (2x SPI IMUs, 2x I2C Compass). The IMUs have a relatively high data rate over SPI-- 20 bytes per reading, 1khz, 2khz, up to 8khz ODR. I would like some assurance before I continue down this path, that this would be a supported/recommended use case. I've understood that the various I2C devices shouldn't be any issue, but I'm concerned about the SPI devices. 

Any ideas?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.