Post Go back to editing

640x480 30Hz Configuration

Thread Summary

The user is troubleshooting a 640x480 30Hz camera sensor with the ADV7513 HDMI transmitter, where no image appears on the monitor. The final answer suggests configuring pixel repetition in register 0x3B and 0x3C to increase the pixel clock to meet the HDMI minimum of 20 MHz. The user should set 0x3C to 0x08 for 2x clock and 4:3 aspect ratio, and ensure the AVI info frame is correctly configured to handle the pixel repetition.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV7513

Hi,

Our camera sensor is 640x480 30Hz only. Below is my configuration so far, but no image on monitor. I think I need to configure pixel repetition in register 0x3B; I've tried a few different setting, but no luck. With the code in it's current state the 'main loop' section also shows pll locked and hpd detected.

void AppEntry( void )

{

uint32_t nCount = 0;

uint8_t nReg;

uint8_t nMode;

uint8_t nReg1, nReg2, nReg3;

//

// Power LED ON, status LED OFF

//

HAL_GPIO_WritePin( GPIOA, LED_PWR_Pin, GPIO_PIN_RESET );

HAL_GPIO_WritePin( GPIOA, LED_STATE_Pin, GPIO_PIN_SET );

//

// Check device is ready and we can talk to it

//

while( true )

{

HAL_StatusTypeDef hal_result;

hal_result = HAL_I2C_IsDeviceReady(

&hi2c1,

( uint16_t ) ( sg_nI2CAdds << 1 ) | 0x01,

3u,

200u

);

if ( hal_result == HAL_OK )

{

break;

}

HAL_Delay( 500 );

// Hard error after 5s.

nCount++;

if ( nCount == 10 )

{

Error_Halt( );

}

}

// === Power / reset ===

WriteReg(0x41, 0x10); // Power up

WriteReg(0x98, 0x03); // Required settings per ADI guide

WriteReg(0x9A, 0xE0);

WriteReg(0x9C, 0x30);

WriteReg(0x9D, 0x61); // Pixel clock divide = /1 (0x61 = ÷1, 27 MHz in)

WriteReg(0xA2, 0xA4);

WriteReg(0xA3, 0xA4);

WriteReg(0xE0, 0xD0);

WriteReg(0xF9, 0x00);

// === Input format ===

WriteReg(0x15, 0x04); // YCbCr 4:2:2, embedded sync

WriteReg(0x16, 0xB8); // 8-bit, style 1 (BT.656), input edge = rising

WriteReg(0x17, 0x02); // 4:3 aspect, DE generator enabled

WriteReg(0x48, 0x00); // Justification evenly distributed

WriteReg(0xD0, 0x00); // Sync pulse mode = case 2 (embedded)

// === Output format ===

WriteReg(0xAF, 0x04); // HDMI mode, no encryption

WriteReg(0x18, 0x06); // CSC disabled (bypass)

// === PLL reset sequence ===

//WriteReg(0x3B, 0x00); // Manual mode, PR = 1x

// === TMDS output ===

WriteReg(0xD6, 0xC0); // TMDS enabled, soft turn-on

//

// Main Loop

//

while( true )

{

//

// Status check

//

nReg1 = ReadReg( 0x41 );

nReg2 = ReadReg( 0x42 );

nReg3 = ReadReg( 0x9E );

if (( nReg1 & 0x10 ) && // Power EN

(( nReg2 & 0xF0 ) == 0xF0 ) && // HDMI status

( nReg3 & 0x10 )) // PLL Lock

{

// LED on

HAL_GPIO_WritePin( GPIOA, LED_STATE_Pin, GPIO_PIN_RESET );

}

else

{

// LED off

HAL_GPIO_WritePin( GPIOA, LED_STATE_Pin, GPIO_PIN_SET );

}

//

// Debug (use breakpoint)

//

// Detected input formats

nReg = ReadReg( 0x3E );

nReg = ReadReg( 0x3F );

nReg = ReadReg( 0x3B );

nReg = ReadReg( 0x3C );

}

}

Parents
  • Hi,

      Yes, Pixel repetition needs to be configured by using register '0x3B', since the pixel clock for 640x480@30Hz is '13 MHz'.

      Kindly note that it is not possible to send this clock, as the minimum requirement is 20 MHz in HDMI. Please refer section 4.3.4 for more details in ADV7511W programming guide at Generated by RMapGen

    Note: Pixel repetition factor is adjusted to meet the bandwidth requirements (To increase the pixel clock to meet the minimum specified clock frequency)

             Pixel repetition is used to get the TMDS clock above the spec'd minimum of 20MHz. When using pixel repetition the sink would need to ignore the duplicated pixels to get back down to a 320x426p60 format. Note the AVI info frame carries the pixel repetition information so the sink can respond correctly.

    Thanks,

    Poornima

  • Hi,

    Thank you for your reply. Could you walk me through each of the register settings to get 0x3B, 0x3C and 0x9D? I've tried a few educated guesses but no luck so far. I.e. nothing on monitor and register 0x3E reads back 0x00.

    Notes
    Sensor format: 640x480, 30Hz, BT.656, YCbCr 4:2:2, 8-bit data connected to Data[15:8] of ADV7513, embedded syncs, 27MHz clock frequency (measured).

    Current register settings:

    WriteReg(0x41, 0x10); // Power up

    WriteReg(0x98, 0x03); // Required settings per ADI guide

    WriteReg(0x9A, 0xE0);

    WriteReg(0x9C, 0x30);

    //WriteReg(0xA4, 0x40); // Enable divide by 2/4 output

    WriteReg(0x9D, 0x61); // Pixel clock not divided. PCLK = 27MHz

    WriteReg(0xA2, 0xA4);

    WriteReg(0xA3, 0xA4);

    WriteReg(0xE0, 0xD0);

    WriteReg(0xF9, 0x00);

    // === Input format ===

    WriteReg(0x15, 0x04); // YCbCr 4:2:2, embedded sync, 2x pixel clock

    WriteReg(0x16, 0xB9 ); // 8-bit, style 1 (BT.656), input edge = falling

    WriteReg(0x17, 0x03); // 4:3 aspect, DE generator enabled

    WriteReg(0x48, 0x00); // Justification evenly distributed

    WriteReg(0xD0, 0x00); // Sync pulse mode = case 2 (embedded)

    // === Output format ===

    WriteReg(0xAF, 0x04); // HDMI mode, no encryption

    WriteReg(0x18, 0x06); // CSC disabled (bypass)

    // === Pixel Repetition ===

    WriteReg(0x3B, 0xCA); // PR Mode = manual

    WriteReg(0x3C, 0x01); // Manual VIC = VGA 4:3

    // === TMDS output ===

    WriteReg(0xD6, 0xC0); // HDP always high, soft turn-on disabled



Reply
  • Hi,

    Thank you for your reply. Could you walk me through each of the register settings to get 0x3B, 0x3C and 0x9D? I've tried a few educated guesses but no luck so far. I.e. nothing on monitor and register 0x3E reads back 0x00.

    Notes
    Sensor format: 640x480, 30Hz, BT.656, YCbCr 4:2:2, 8-bit data connected to Data[15:8] of ADV7513, embedded syncs, 27MHz clock frequency (measured).

    Current register settings:

    WriteReg(0x41, 0x10); // Power up

    WriteReg(0x98, 0x03); // Required settings per ADI guide

    WriteReg(0x9A, 0xE0);

    WriteReg(0x9C, 0x30);

    //WriteReg(0xA4, 0x40); // Enable divide by 2/4 output

    WriteReg(0x9D, 0x61); // Pixel clock not divided. PCLK = 27MHz

    WriteReg(0xA2, 0xA4);

    WriteReg(0xA3, 0xA4);

    WriteReg(0xE0, 0xD0);

    WriteReg(0xF9, 0x00);

    // === Input format ===

    WriteReg(0x15, 0x04); // YCbCr 4:2:2, embedded sync, 2x pixel clock

    WriteReg(0x16, 0xB9 ); // 8-bit, style 1 (BT.656), input edge = falling

    WriteReg(0x17, 0x03); // 4:3 aspect, DE generator enabled

    WriteReg(0x48, 0x00); // Justification evenly distributed

    WriteReg(0xD0, 0x00); // Sync pulse mode = case 2 (embedded)

    // === Output format ===

    WriteReg(0xAF, 0x04); // HDMI mode, no encryption

    WriteReg(0x18, 0x06); // CSC disabled (bypass)

    // === Pixel Repetition ===

    WriteReg(0x3B, 0xCA); // PR Mode = manual

    WriteReg(0x3C, 0x01); // Manual VIC = VGA 4:3

    // === TMDS output ===

    WriteReg(0xD6, 0xC0); // HDP always high, soft turn-on disabled



Children
  • Hi,

       Kindly note that, 'VIC 1' corresponds to '640x480p'@60Hz but your video format seems '640x480p'@30Hz. Please configure it with different value and let us know,

    // === Pixel Repetition ===

       WriteReg (0x3C, 0x08); //240p-60, 2x Clk, 4:3 

    In the manual pixel repeat selection case, the VIC sent in the AVI info frame will need to be set in register 0x3C. The multiplication of the input clock must be programmed in 0x3B[6:5], and the pixel repeat value sent to the Rx must be programmed in 0x3B[4:3]. 

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.