Post Go back to editing

CLK IN Crosstalk

Thread Summary

The user is concerned about potential crosstalk issues between a 165 MHz clock signal and parallel video signals on a board. The final answer confirms that the ADV7511 IC can tolerate input voltages between 1.8V and 3.3V, and as long as the high-level input voltage remains within these limits, crosstalk should not cause issues. The accompanying answer suggests referring to the ADV7511 evaluation layout and HDMI layout guidelines for further routing recommendations.
AI Generated Content
Category: Hardware
Product Number: ADV7511

Hello, I was wondering if the clock in signal will have issues with crosstalk. 

On my board I have put the clock in signal on a Board to Board connector pin that is next to the video in parallel signals. The clock in pin on the IC is also next to the video signals, will it create crosstalk issues?

The datasheet says to keep high speed lines away from the clock signal but the clock pin on the IC is right next to the 165 MHz video in signals. Do you mean non clock synced signals?

  • Hi,

       Please refer our ADV7511 layout at https://www.analog.com/media/en/technical-documentation/evaluation-documentation/adv7511_adv7343_eval_layout.pdf for the dimension of the 'Clock in and Video' Signals.

      Also this FAQ presents a general guideline to laying out HDMI traces on circuit boards HDMI Layout Guideline 

    Thanks,

    Poornima S

  • Could I know the rise times at least, so I can try to calculate the crosstalk? Rise time is not mentioned in the HW Guide. I presume it depends on the mode but an estimate/minimum/maximum would be nice.

    The routing document you sent is not that helpful because it is different than my use case. Im routing the 165 MHz parallel input lines to an FPGA SOM and all the traces on the SOM are differential pairs so Im really concerned about crosstalk.

    edit: the HW Guide says that the logic voltage is between 1.8v and 3.3v. Does it depend on the mode? Meaning does the IC expect either 1.8V and 3.3V or anything in between? if anything in between then the coupled crosstalk voltage won't have any effect

    edit2: others asked about rise times and you said to use ibis models however all links to get the ibis models are not working. i prefer not to use an ibis model because ive never used one before and probably dont have the software to do so. so i would prefer an estimate

  • Hi,

    The HW Guide says that the logic voltage is between 1.8v and 3.3v. Does it depend on the mode? Meaning does the IC expect either 1.8V and 3.3V or anything in between? if anything in between then the coupled crosstalk voltage won't have any effect

            The part does not cause any issue as long as it operates according to the specification.

            According to the hardware User guide electrical specifications for digital inputs Vih_min = 1.35V and Vih_max = 3.5V.  As long as the input voltage high is within those limits it should work.

           AVDD, DVDD, PVDD, PLVDD needs to be 1.8V

          MVDD (pin 47) needs to be 3.3V

          The digital inputs are 3.3V tolerant.

    Kindly refer at  ADV7511 video inputs accept logic levels from 1.8 V to 3.3 V?

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.