Hello,
Question about AHD and 7280A, Can it successfully support higher resolution @50Hz even if not 'standard' (lower frame rate). I ask before going into some changes for WxH setting in the lower driver configuration. Just reading Status register 1,2 and 3 looks not obvious if internal circuitry adjusted to H/V Sync, INST_HLOCK(1), SD_OP_50Hz(1)
[ 172.999512] adv7180 [status]:0x8a:00:49h
[ 261.199012] adv7180 [status]:0x8a:00:48h
[ 2483.060258] adv7180 [status]:0x0f:00:69h
Thanks, Guy.