Post Go back to editing

AD724 Luma/Chroma outputs do not meet SMPTE standard for NTSC

Thread Summary

The user is experiencing issues with the AD724 not meeting SMPTE NTSC luma/chroma values for 75% colorbars, even with a precise 14.31818 MHz clock and synchronous operation. The final answer suggests evaluating the AD724 on the official evaluation board to confirm adherence to SMPTE standards, as no specific test results are available. The user has already confirmed their system is correctly configured and synchronized, but still observes significant chroma discrepancies.
AI Generated Content
Category: Hardware
Product Number: AD724

Hello, I've got a number of questions but the core issue that I'm seeing is that the luma/chroma values that the AD724 puts out for NTSC do not meet the SMPTE spec (tested with 75% colorbars).

If I go as far as to tweak RGB values for the color pattern to fix luma, chroma goes off. Chroma (especially for cyan, green, magenta, and red) are all giving me values about 15-18 IRE less than they should.

Finally, I've seen consistent noise that looks sinusoidal on the chroma output. I went as far as to use an oscilloscope to measure the period of this sinusoidal noise and it appears to match the 3.58 MHz subcarrier frequency. Our circuit design mostly matches the example one on the AD724 datasheet (figure 16) with the difference that we use a ADV7125 instead of a ADV7120 and we drive inputs to the ADV7125 using a TI SN65LVDS822RGZR driven by a FPGA. It seems to me that this noise may come from the asynchronous subcarrier operation.

For some additional context, I measured using a VM700T on both composite and S-Video outputs of a custom solution.

To consolidate my questions, they are as follows:

  • Is the AD724 meant to adhere to the SMPTE spec for NTSC?
  • Is the increased jitter as a result of asynchronous operation referenced in the "Synchronous vs. Asynchronous Operation" section of the datasheet noise directly from the subcarrier frequency?
  • The specifications of the AD724 are noted to be for a "FSC synchronous clock". Is there information about performance of the AD724 with asynchronous information? I don't know how much "worse" asynchronous operation is compared to synchronous operation and nothing in the datasheet gives a quantitative depiction of that.
Parents
  • Hi,

      Please find below comment for your queries,

    • Is the AD724 meant to adhere to the SMPTE spec for NTSC ?

                  I believe AD724 adhere to the SMPTE170M (i.e AD724 outputs NTSC signals that conform to SMPTE 170M). As per specification Most of the more common variants of NTSC and PAL are supported. There are, however, two known specific standards not supported. These are NTSC 4.43 and M-PAL.

                  Kindly note that, AD723/4/5 requires interlaced RGB on its inputs & it do not perform any advanced video processing, So it's interlaced to interlaced.

              Please make sure with your input.

                 AD725 can be used to convert the analog RGB output from a personal computer’s VGA card to the NTSC or PAL television standards.
                 To accomplish this it is important to understand that the AD725 requires interlaced RGB video and clock rates that are consistent with those required by the television standards.
                  In most computers the default output is a non-interlaced RGB signal at a frame rate higher than used by either NTSC or PAL.

    • Is the increased jitter as a result of asynchronous operation referenced in the "Synchronous vs. Asynchronous Operation" section of the datasheet noise directly from the subcarrier frequency ?

                     Yes, AD724 datasheet states that phase drift between luminance and chroma paths in async mode leads to modulation jitter and visible chroma distortion.

                     Also inorder to Avoid Asynchronous Operation Jitter in AD724,
                          Try to use an External Clock (CLKIN) instead of Internal Crystal Oscillator and don’t use the XTAL1/XTAL2 pins (this puts you in asynchronous mode).Instead, drive the CLKIN pin with a 3.579545 MHz (NTSC) subcarrier clock.

                     Please check this AD724 operating instructions https://www.analog.com/media/en/technical-documentation/evaluation-documentation/AD724_eval_board_instructions.pdf

    • The specifications of the AD724 are noted to be for a "FSC synchronous clock". Is there information about performance of the AD724 with asynchronous information? I don't know how much "worse" asynchronous operation is compared to synchronous operation and nothing in the datasheet gives a quantitative depiction of that.

                   Please refer this FAQ  AD724: FAQ ,  AD725: FAQ 

                                       

    Thanks,

    Poornima

  • Hi Poornima - thank you for the response. There isn't anything in the AD724 or AD725 FAQs which tells me anything more about the performance of the AD724 during asynchronous operation.

    I am getting an output NTSC video. My inputs and outputs of the AD724 look good. I'm able to see the S-Video/composite outputs on monitors. I'm not struggling to get a video output. I am struggling to get the AD724 to put out correct chroma values when giving it a SMPTE 75% colorbars test pattern.

    I tuned my external clock and used a frequency/clock counter to confirm my FIN/Fsc clock was getting 14.31818 MHz while SELECT was pulled high and also tested with 3.579545 MHz with SELECT pulled low. In both operations it seems like my chroma values are still somewhat substantially off.

    At this point I don't know if the chroma values put out by the AD724 that do not match the 75% colorbars SMPTE test pattern expected luma/chroma values are because the asynchronous operations results in substantially worse chroma, if there is something for me to tweak on the board, or if the AD724 simply does not adhere to the SMPTE specification well enough. Any information that I can get which gives me a clear indication of the AD724's reduced performance as a result of asynchronous operation would be helpful since it does not seem like this information has been documented in any quantitative fashion in either the FAQs or the datasheet.

    The closest thing I have to something quantitative is this from the datasheet: "However, in asynchronous systems the sync to burst position can change line to line by as much as 140 ns (the period of a 2FSC clock cycle) due to the fact that the burst flag is generated from a clocked CSYNC while the sync is injected unclocked. This phenomenon may or may not create visual artifacts in some highend video systems."

    I have seen the variability of the sync to burst using my VM700T, but I don't have an idea of what the end result of this variability may be on my chroma outputs. That's what I need to know.

  • Poornima, do you have any information on how the synchronization signals and RGB outputs are generated such that they are synchronous to the 3.579545 MHz clock? The pixel clock for NTSC is 13.5 MHz. I might be able to get away with using the 4xFsc of 14.31818 MHz as my RGB pixel clock, but that will result in a somewhat non-standard NTSC output.

  • Hi,

    Please check with below response and let us know,

     I might be able to get away with using the 4xFsc of 14.31818 MHz as my RGB pixel clock, but that will result in a somewhat non-standard NTSC output.

      As per expert comment, The accuracy of the external crystal oscillator reference at 4FSC will be better than +/- 100 ppm, so the ambiguity due to this tolerance will also be negligible.

    Also, As per specification Fsc frequency for NTSC is 3.579545 MHz for and 4.433618 MHz for PAL.

    Do you have any information on how the synchronization signals and RGB outputs are generated such that they are synchronous to the 3.579545 MHz clock? 

    Please refer below for generating the synchronization signals and RGB output,

     - Using a pixel clock (e.g., 14.31818 MHz) to drive timing.
     - Counting clock cycles to determine position in a scanline (horizontal timing) and which scanline you're on (vertical timing) 
     - Generating HSYNC and VSYNC based on known timing values (Correct intervals)
     - Enable RGB output only during the active region of the screen.
     - Keep everything synchronized with the base clock.

    Thanks,

    Poornima

  • Hi Poornima, it's been a while!

    I am now working with a system that:

    • Uses a externally driven, 0ppb error 14.31818 MHz clock that functions as both my pixel clock as well as my subcarrier frequency input
    • Generates timing signals based on known timing values
    • Keeps RGB output only during the active region of the screen
    • Keeps everything synchronized with the base clock.

    Unfortunately, my IRE values are not within the SMPTE standard still (measured using a VM700T). I get:

    Color Luma (IRE) Chroma (IRE)

    Gray

    69.9 1.4

    Yellow

    62.1 52.0
    Cyan 50.3 72.5
    Green 43.1 68.0
    Magenta 32.4 70.6
    Red 24.8 73.3
    Blue 14.2 54.3
    Black 7.3 2.1

    SMPTE colorbars (75%) are meant to have the following values:

    Color Luma (IRE) Chroma (IRE)

    Gray

    76.9 0.0
    Yellow 69.0 62.1
    Cyan 56.1 87.7
    Green 48.2 81.9
    Magenta 36.2 81.9
    Red 28.2 87.7
    Blue 15.4 62.1
    Black 7.5 0.0

    It looks to me like in the ideal conditions, the AD724 is falling short of being within reasonable range of the SMPTE standard.

    Is there any way to amend this in code or electronics? Am I missing something?

  • I'd like a response if possible so that I can know what I may be able to do to get the AD724 to output in a way that aligns with the SMPTE standard. Otherwise, I will verify that the answer is simply that the AD724 does not actually properly adhere to the SMPTE standard.

  • Hi,

      Apologies for the delayed response. I have been attending internal training.

     It's better to confirm by evaluating the same IRE with our AD724 evaluation board.

    Thanks,

    Poornima

  • Hi Poornima, that's a great idea! What are the IRE values that are read off of the AD724 evaluation board?

  • Hi,

      When using the AD724 Evaluation Board, the IRE values that can be read off from the AD724 video output will depend on the input RGB signals and how the board is configured. 

     Kindly refer below snap, This table shows the associated current,voltage and IRE relationships for the various video standards at https://www.analog.com/media/en/technical-documentation/application-notes/478955693AN205.pdf

      Also refer AD724 board instructions details at https://www.analog.com/media/en/technical-documentation/evaluation-documentation/AD724_eval_board_instructions.pdf

      https://www.analog.com/media/en/evaluation-boards-kits/evaluation-software/357707021AD72x_EVB.zip

    Thanks,

    Poornima

  • Hi Poornima, yes - IRE values depend on what the driving RGB signals are providing. Unfortunately, the only thing that table tells me is the minimum and maximum IRE values for luma per video standard.

    I'm holding a copy of SMPTE-170M in front of me now. Pages 17-18 provide the IRE values for luma and chroma for 75% and 100% SMPTE colorbars. The only thing the AN-205 application note table tells me is the white->black IRE value. If the AD724 is SMPTE compliant, I would hope that Analog Devices has a copy of testing done with SMPTE colorbars that show a clear representation of luma/chroma values for each color.

    I'm not interested in buying, programming, and then effectively running a verification test on a $327 eval board. I have my own verification tests to run on my own product.

    If Analog Devices does not have test results for the AD724 luma/chroma voltage/IRE per SMPTE color pattern color, my conclusion will be that Analog Devices ensured that the AD724 could get a 7.5-100 IRE black-white luma on NTSC with undocumented respective RGB values. With no evidence of IRE values for individual colors (or any chroma values for that matter), the AD724 does not adhere to the SMPTE-170M standard.

    Please let me know if Analog Devices has evidence of testing to adhere to SMPTE luma/chroma values.

  • Hi,

      Please let me know if Analog Devices has evidence of testing to adhere to SMPTE luma/chroma values.

            We can confirm this only by checking it on our evaluation board, as we currently have no evidence other than what is mentioned in the AD724 specification manuals.

    Thanks,

    Poornima

  • Ok, thank you for all of your help with this Poornima.

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.