Post Go back to editing

MAX7312 V1.0.0 EVKit SW cannot recognize the I2C device of MAX7312EvKit board

Category: Hardware
Product Number: MAX7312

At the beginning, it was able to successfully connect and control the LED lights through IO.

Unable to connect properly now, JU1-JU5's jumper settings are the same as before, and the USB port can also be recognized on the device manager, but still unable to connect. May I ask what the problem is?