Post Go back to editing

How to use the undocumented "DIGITAL CVBS INPUT" from the ADV7802

Thread Summary

The user is designing a board using the ADV7802 chip and wants to use the digital CVBS input mode. The final answer suggests that a hidden MUX or undocumented register can select the CVBS decoder's input source as digital (12-bit parallel) over D[11:0], clocked at 28.63636 MHz. For early design, it's recommended to route D[11:0] and CLKIN, and add a test header or mux to toggle between analog and digital CVBS paths. The accompanying answers clarify that there are no specific registers for this mode and suggest connecting the MCU/FPGA to CLKIN(78) for testing.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV7802

Hello , I'm an independent developer working on designing a board using your ADV7802 chip.

By looking at the internal diagram, I can see that the digital input are muxed at the same place as the digital output of the different 12bit ADC.

i also noticed in the datasheet that there is a mention of a "digital cvbs input mode" on the pin 78 (CLKIN).

It turns out I'm part of a project where I work with digital cvbs file. So i would love if i could use an mcu or an fpga to feed my digital cvbs to the chip so i could leverage his 3D decoder and 3D NR without going to analogue.

Could you guide me on how i could achieve this goal and how i could use that digital cvbs input mode.

I would really appreciate your help, thanks.

Parents
  • Hi,

      Kindly note that, There is no register which is available for 'digital cvbs input mode' so just connect your MCU/FPGA  with CLKIN(78) pin and let us know.

    Thanks,

    Poornima

  • the CLKIN jusst mention it could be used with the digital cvbs input mode but doesn't say it is an input.

    i supose there is a way to use some reserved register to mux the digital cvbs to the CVBS processing core. but i would also have to know the exact format used by the decoder and how to let it accept 12 bit data on the digital input. i'm also in the design phase, so i can't test without knowing how that should be implemented. I suppose the digital cvbs input must have been used during the design phase to test the comb filter but as then be left undocumented other that that mention on the screenshot.

Reply
  • the CLKIN jusst mention it could be used with the digital cvbs input mode but doesn't say it is an input.

    i supose there is a way to use some reserved register to mux the digital cvbs to the CVBS processing core. but i would also have to know the exact format used by the decoder and how to let it accept 12 bit data on the digital input. i'm also in the design phase, so i can't test without knowing how that should be implemented. I suppose the digital cvbs input must have been used during the design phase to test the comb filter but as then be left undocumented other that that mention on the screenshot.

Children
  • Hi,

    Kindly note that, We don't any register details other than what available in the manuals.

    A hidden MUX or undocumented register selects the CVBS decoder’s input source as digital (parallel) instead of analog So i believe, We can make it by giving 12-bit digital CVBS over digital input interface D[11:0].

    If you're in early design:
    Leave flexibility in your layout (route D[11:0] and CLKIN).
    Add a test header or mux to toggle between analog and digital CVBS paths.
    Design assuming 12-bit CVBS over D[11:0], clocked at 28.63636 MHz (as per XTAL).

    Thanks,

    Poornima