Post Go back to editing

7604 VSYNC pulse width

Thread Summary

The user reports an issue with the ADV7604 in HDMI-GR mode where the VSYNC signal width becomes abnormally large (about 50% duty cycle) when changing input resolution and/or FPS, particularly with 1024x2048/60Hz. The issue resolves after resetting the ADV7604. The support engineer suggests checking the source (GPU) output timing and ensuring the V_LOCKED and TMDS_LCK status registers are monitored during format changes. The user confirms that a parallel-connected display works correctly, indicating the issue may be specific to the ADV7604 and the application circuitry.
AI Generated Content
Category: Hardware
Product Number: ADV7604

Hi,

ADV7604 in HDMI-GR mode. When changing input resolution and/or FPS sometimes the width of VSYNC signal is very big (approx. half of frame) - VSYNC duty cycle is about 50%, period VSYNC is OK. After reset applying the width of VSYNC returns to normal.  What could be the reason of a such behavior?   Is it possible to diagnose it in any way?   

  • Hi,

      If Possible, Please share your register configuration.

      Also monitor the 'V_LOCKED_RAW, V_LOCKED_ST, TMDS_LCK_x_RAW' during that case and also ensure the recommended writes as per this document "ADV7604_RecommendedSettings_Rev2.5.pdf"

      Generally, format changes can cause V_LOCK to unlock it may take a frame or 2 for the chip to lock on to the new format. During this interval you can either free run or black screen the video.

    Please check with other source device since some source may not generate a Stable VSYNC Signal during resolution change

    Thanks,

    Poornima

  • Hi,

    here is our register configuration:

    ;AD7604
    40 0C 42 ; Power up part and power down VDP
    40 00 07 ; VID_STD=00111b for autographics mode
    40 15 BE ; Tristate all outputs from video core
    68 1A 1A ; Mute audio
    68 01 78 ; Open termination
    40 F7 66 ; DPP Address to 66
    40 01 06 ; Prim_Mode =110b HDMI-GR
    40 02 12 ; RGB 0-255 out, Set ALT_DATA_SAT --- EZ ---
    40 03 40 ; 24 bit SDR 444 Mode 0 
    40 05 28 ; AV Codes Off, blank data
    40 06 A1 ; Inv LLC 
    40 0B 44 ; Power down ESDP block
    40 14 7F ; Drive strength adjustment
    40 15 80 ; Disable Tristate of Pins
    40 33 60 ; LLC DLL Mux Enable
    44 69 00 ; Disable CP CSC --- EZ ---
    44 6C D0 ; CLMP_A_MAN and CLMP_BC_MAN set to 0 --- EZ ---
    44 85 0B ; Disable Autodetectmode for Sync_Source for CH1. Force CH1 to use seperate HS & VS.
    44 BA 00 ; HDMI FreeRun disable
    44 CF 01 ; Power off macrovision
    4C 00 FF ; Power Down ADC's and there associated clocks
    4C 01 FE ; Power down ref buffer/bandgap/clamps/sync strippers/input mux/output buffer
    4C 13 93 ; Set LLC DLL Phase
    4C B5 01 ; Setting MCLK to 256Fs
    4C C8 40 ; ADI recommended setting
    68 01 00 ; Enable clock terminators
    68 0D 84 ; ADI recommended write
    68 15 03 ; Set Audio FIFO Mute Masks
    68 1A 0A ; Set Unmute Delay to 1_5 sec
    68 3D 10 ; ADI Recommended Setting
    68 3E 39 ; ADI recommended setting
    68 48 06 ; Set Audio FIFO reset
    68 57 B6 ; Enable dynamic PLL control
    68 58 03 ; Recommended PLL setting
    68 59 A3 ; ADI recommended setting
    68 8C A3 ; ....dflt.....
    68 8D 18 ; ADI recommended equalizer setting.
    68 8E 34 ; ADI recommended equalizer setting
    68 93 8B ; Equaliser ADI recommended setting
    68 94 2D ; Equaliser ADI recommended setting
    68 96 01 ; Enable automatic EQ changing

    V_LOCKED_RAW and TMDS_CLK_x_RAW indicate locked state (1) when VSYNC is not standard ("error" state). What is the meaning of V_LOCKED_ST?

    Thanks

    Vilem

  • Hi,

       Please let us know the reason for tristate(high impedance) the "Pixel bus / LLC Pin / Sync out Pins" (i.e 40 15 BE).

       Also its seems, the 'VID_STD' register has not been configured to graphics mode (40 00 07 ; VID_STD=00111b for autographic mode) and let us know your graphic mode resolution.

    V_LOCKED_ST - Latched status for the vertical sync filter locked interrupt. Once set, this bit will remain high until the interrupt is cleared via V_LOCKED_CLR. This bit is only valid if enabled via the corresponding INT1 or INT2 interrupt mask bit.

    V_LOCKED_ST is a latched version of V_LOCKED_RAW.

    Kindly note that, "_ST is the latched  version of _RAW " _CLEAR clears the _ST bit. 

                                 ST bit is the latched version of RAW so RAW could be low while ST is high.

    Thanks,

    Poornima

  • Hi,

    yes, you are right, there is no reason for 40 15 BE, because BE is default value and there is no reason why to  write it. On the row nr. 14 there is 40 15 80 write for disable tristate of pins. 

    Why do you think the VID_STD has not been configured to autographics mode? It was the only way how to make 7604 operational with 1024x2048 resolution. We solved in with ADI support on Apr 17 2024.

    Thank you for explanation of V_LOCKED_ST.

    Thanks

    Vilem

  • Hi,

      Please let us know, In which manual are you referring to configure the 'VID_STD' register ?

    Thanks,

    Poornima

  • Hi,

    here is a part of communication that was carried approx. 1 year ago:

    Hi,

    Yes. Autographic mode is available also for digital (DVI) input.
    For selecting autographic mode, we would need to set PRIM_MODE[3:0]: 0x02 and VID_STD[5:0]: 0x07. 
    Thanks,
    Dharani S
    .............

    Hi,

    now it seems we have found the configuration that works well  We programmed video standard, as you adviced, to auto-graphics. But primary mode we programmed to PRIM_MODE[3:0]=0b0110 (HDMI-GR). In addition we wrote (CP map, 0x85)=0xB (disable Autodetectmode for Sync_Source for CH1, force CH1 to use seperate HS & VS). Yes, it works, but I´m a little confused, because it doesnn´t fully conform to the 7604 hw documentation.

    Thanks

    Vilem

    Yes, to say the truth, this configirution we use for 1024x2048 is not apparently documented......? 
    Thanks
    Vilem
  • Hi,

      Please find ADV7604 hardware manual here /cfs-file/__key/communityserver-discussions-components-files/331/ADV7604-HW-RvF-Aug_2700_10.pdf

       At first please check the graphic mode resolution which is available in the 'VID_STD' register(Refer Page 49) and let us know the result.

    Thanks,

    Poornima

  • Hi,

    I tested two configurations:

    1. PRIM_MODE=0x6 (0b0110) - HDMI-GR; VID_STD[3:0]=0b00111 (reserved) - autographics ?

    2. PRIM_MODE=0x6 (0b0110) - HDMI-GR; VID_STD[3:0]=0b00110 (1280x1024/75Hz)

    It seems both configurations work with our 1024x2048/60Hz. Is really autographics mode available for DVI/HDMI input? 

    Thanks

    Vilem 

  • Hi,

      Yes, Autographic mode is available for both DVI/HDMI input.

      Please refer DVI script configuration at ez.analog.com/.../6114.ADV7604IO_5F00_ADV7604CP_5F00_ADV7604AFE_5F00_ADV7604HDMI_5F00_ADV7341B_2D00_VER.1.4c_5F00_RevA.txt.zip

    Thanks,

    Poornima

  • Hi,

    unfortunately, I don´t understand. One of two notices about autographic mode is for example here:

    ##Graphics - UXGA, 1600x1200##
    :Graphics-8.2 1600x1200 _@ 60 162.000MHz Out through DVI:
    50 20 10 ; FPGA HPD on TX
    40 0C 42 ; Power up part and Power down VDP
    40 00 16 ; VID_STD=00111b for autographics mode

    ......

    But for aotographics mode there should be 40 00 07 and not 40 00 16.......??

    By the way, what about original topic - the width of VSYNC signal? This still sometimes appears and the graphics mode has no influence on it.

    Thanks

    Vilem