Post Go back to editing

Request for Custom Design Clarification- ADV7282AWBCPZ-M

Category: Hardware
Product Number: ADV7282AWBCPZ-M, ADV7282A

Hi,

We are designing our custom board with ADV7282AWBCPZ-M. Kindly clarify the below queries.

This is the Summary:

This is reference I used to design the custom board with ADV7282AWBCPZ-M [Please find the attached Pdf file]

 

  1. I removed the entire USB page (please refer to the diagram in reference pdf). Instead, I provided a two-pin header for both SDA and SCLK. This will be used for flashing the ADV7282AWBCPZ-M from an external host like an Arduino or Raspberry Pi. Please confirm whether this is sufficient for flashing the ADV7282AWBCPZ-M or if an EEPROM or external flash is required.
  2. I also noticed that the reference design for the ADV7282AWBCPZ-M does not follow a power sequence for the reset and power-down functions (for the reset pin, they provide a physical switch, and for power down, they simply connect it to a high signal through a 4.7K resistor and to ground through a 0-ohm resistor). Should I use that circuit for the reset and power-down functions, or should I use the one I’ve attached below? 
  3. Regarding the DIAG pin, I made the connection as shown below and connected DIAG1 and DIAG2 to the DIAG pins of the ADV7282AWBCPZ-M. Kindly confirm this. (Our input signals are single-ended.)  
  4. For the power sequence: We have a 3.3V rail, and the 1.8V rail powers up after it. Please confirm if this sequence is correct for the ADV7282AWBCPZ-M, and for the reset and power-down sequence, please refer to point 2.
  5. How do I program the ADV7282AWBCPZ-M with an external I2C master? Does it require any specific software, driver, or script? Could you share any documentation or instructions on how to flash the new ICs with an external master? Or, can I follow the same procedure as your evaluation board?

 

Regards,

Nitheesh

Parents Reply
  • Hi,

    Thanks For Your Response.

    Please confirm the below queries.

    • Should I use the same program [Evaluation Board Program] for the new ICs also? There's no need to modify anything, right, since we only have two analog single-ended inputs? Or do we need to make any modifications for these types of hardware changes?

    • If the evaluation board script file is sufficient, we don't need any external flash, right? The ADV7282AWBCPZ-M itself should be enough to store this script file program, correct?

    • Additionally, I referred to the reference design you suggested in the previous reply, and there is no circuit for power delay. In that design, 3.3V and 1.8V are derived directly from 7.4V. In our case, we have a 3.3V output regulator, and from the 3.3V output, we generate 1.8V. Therefore, 1.8V powers up only after 3.3V. This power sequence should be sufficient, right?

    Please find the attached circuit diagram. kindly review and share your comments.

    PDF

    Regards,

    Nitheesh

Children