| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 28 hours |
Open | |
MAX6955
Production
The MAX6955 is a compact display driver that interfaces microprocessors to a mix of 7-segment, 14-segment, and 16-segment LED displays through an I2C-compatible...
Datasheet
MAX6955 on Analog.com
On the 7 segment application note page
Figure 1 is too low resolution to be able to read.
When can we find a high resolution version of this image?
Hi,
We are not aware about this part. For more information, please visit one of the technical support pages on our newly integrated website below for assistance with Maxim Integrated products.
I have lodged a ticket CS-438913-R4J3V7 but no-one is providing the answer.
The MAX6955 is one of your LED driver chips.
Can you please provide a higher resolution version of figure 1 as per the link provided for the application note page
Hi,
Please find the high resolution MAX6954 7-segment application circuit image,

Thanks,
Poornima
Hi Poornima, thankyou for supplying the 14-segment LED diagram.
The request is for the 7-segment LED diagram as shown in the application note link for figure 1. As published this image is low resolution and the pin numbers cannot be seen.

Ben
Hi,
Please refer Page38 for getting the high resolution image of MAX6955 7-segment application circuit at MAX6955 DS-B&F-Rebranded
Reference MAX6955 Datasheet and Product Info | Analog Devices
Thanks,
Poornima
Hi Poornima.
The application diagram in the datasheet only shows dual colour 7-segment displays.

The application note is providing additional information that the datasheet does not provide and Figure 1 is critical to that information. The application note figure 1 shows how to connect 16 digits of 7 segment monocolor displays.
If we download the application note as a pdf, there is a hyperlink under Figure 1 to click "For Larger Image". This link is broken.


Can you please locate and provide a copy of Figure 1 in higher resolution so the details within the diagram can be seen?
Thanks
Ben
Hi,
Please check below referred image and note that we don't have any figure other than what we have shared till now.

Kindly try with any 'Scaling' exe in order to rectify the low-resolution image.
Thanks,
Poornima
The datasheet page 36 diagram has an error. It references digits 0a and 0b. Everywhere else in the datasheet they are referenced as 0 and 0a.

I have shown you multiple times the figure 1 image that needs to be improved. This is your webpage and your data. It is your responsibility to provide suitable information for your products.

Please locate the original image, or re-draw it if necessary.
Please fix the 0b incorrect references in the datasheet.
this issue needs to be escalated.
Hi,
This is not in our hand and this need to be check with expert about the Manual related correction & update in the respective part product page.
Thanks,
Poornima
Hi,
This is not in our hand and this need to be check with expert about the Manual related correction & update in the respective part product page.
Thanks,
Poornima