Post Go back to editing

Quick start guide diagram cannot read

Thread Summary

The user requested a high-resolution version of Figure 1 from the MAX6954 7-segment display application note, as the published version is too low resolution to read pin numbers. The support engineer provided a high-resolution image from the MAX6955 datasheet, but it only shows dual-color 7-segment displays. The user clarified that the application note figure is critical and contains errors, requesting the original or a corrected high-resolution version. The support engineer suggested using a scaling tool to improve the image quality and noted that the issue would be escalated.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX6955

On the 7 segment application note page

https://www.analog.com/en/resources/design-notes/quickstart-driving-7segment-displays-with-the-max6954.html

Figure 1 is too low resolution to be able to read.

When can we find a high resolution version of this image?

Parents Reply
  • The datasheet page 36 diagram has an error. It references digits 0a and 0b. Everywhere else in the datasheet they are referenced as 0 and 0a.

    I have shown you multiple times the figure 1 image that needs to be improved. This is your webpage and your data. It is your responsibility to provide suitable information for your products.

    Please locate the original image, or re-draw it if necessary.

    Please fix the 0b incorrect references in the datasheet.

    this issue needs to be escalated.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.