Post Go back to editing

Quick start guide diagram cannot read

Thread Summary

The user requested a high-resolution version of Figure 1 from the MAX6954 7-segment display application note, as the published version is too low resolution to read pin numbers. The support engineer provided a high-resolution image from the MAX6955 datasheet, but it only shows dual-color 7-segment displays. The user clarified that the application note figure is critical and contains errors, requesting the original or a corrected high-resolution version. The support engineer suggested using a scaling tool to improve the image quality and noted that the issue would be escalated.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX6955

On the 7 segment application note page

https://www.analog.com/en/resources/design-notes/quickstart-driving-7segment-displays-with-the-max6954.html

Figure 1 is too low resolution to be able to read.

When can we find a high resolution version of this image?

Parents Reply Children
  • Hi Poornima.

    The application diagram in the datasheet only shows dual colour 7-segment displays.

    The application note is providing additional information that the datasheet does not provide and Figure 1 is critical to that information. The application note figure 1 shows how to connect 16 digits of 7 segment monocolor displays.

    If we download the application note as a pdf, there is a hyperlink under Figure 1 to click "For Larger Image". This link is broken.

    Can you please locate and provide a copy of Figure 1 in higher resolution so the details within the diagram can be seen?

    Thanks

    Ben

  • Hi,

      Please check below referred image and note that we don't have any figure other than what we have shared till now.

      

    Kindly try with any 'Scaling' exe in order to rectify the low-resolution image.

    Thanks,

    Poornima

  • The datasheet page 36 diagram has an error. It references digits 0a and 0b. Everywhere else in the datasheet they are referenced as 0 and 0a.

    I have shown you multiple times the figure 1 image that needs to be improved. This is your webpage and your data. It is your responsibility to provide suitable information for your products.

    Please locate the original image, or re-draw it if necessary.

    Please fix the 0b incorrect references in the datasheet.

    this issue needs to be escalated.

  • Hi,

      This is not in our hand and this need to be check with expert about the Manual related correction & update in the respective part product page.

    Thanks,

    Poornima

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.