Post Go back to editing

Quick start guide diagram cannot read

Thread Summary

The user requested a high-resolution version of Figure 1 from the MAX6954 7-segment display application note, as the published version is too low resolution to read pin numbers. The support engineer provided a high-resolution image from the MAX6955 datasheet, but it only shows dual-color 7-segment displays. The user clarified that the application note figure is critical and contains errors, requesting the original or a corrected high-resolution version. The support engineer suggested using a scaling tool to improve the image quality and noted that the issue would be escalated.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX6955

On the 7 segment application note page

https://www.analog.com/en/resources/design-notes/quickstart-driving-7segment-displays-with-the-max6954.html

Figure 1 is too low resolution to be able to read.

When can we find a high resolution version of this image?

Parents Reply Children