Post Go back to editing

Enabling PLL stop video conversion to CVBS

Category: Hardware
Product Number: ADV7393
We are using ADV7393 to convert digital video stream from DPI to CVBS.
The input video on DPI is SD video stream 720x480 resolution BT656 video standard and 10 DPI data pin connected.
 
We use the next config to enable video stream:
## Use example Table 82. 8-Bit  625i YCrCb In (EAV/SAV), CVBS/Y-C Out but with adjustmen for 10 bits
i2cset -y 1 0x2a 0x17 0x02 # Software reset.
i2cset -y 1 0x2a 0x82 0xC3 # SD PrPb SSAF filter + SD DAC Output 1 (Enable CVBS) + Data Valid
i2cset -y 1 0x2a 0x88 0x10 # 10-bit input enabled.



The problem is that when we enable PLL with the ebove config using the next command, the video stream conversion stops:
i2cset -y 1 0x2a 0x00 0x10 # DAC1 + PLL enable
# Setting 0x00 register value to 0x10
 
What prerequisites or extra steps do we need to make to enable PLL x16?
Parents
  • Hi,

     Please ensure with below 16x PLL configuration been enabled for SD mode since this setting multiplies the input clock frequency by 16, which is typically used for standard definition (SD) video formats.

     As per our default configuration, enable 0x00 register value as 0x1C - All DAC enabled/ PLL enabled(16x) and let us know about the result.

    Thanks,

    Poornima

  • PLL does not work. I tried next steps:

    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x17 0x02 # Software reset.
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x82 0xC3 # SD PrPb SSAF filter + SD DAC Output 1 (Enable CVBS) + Data Valid
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x88 0x10 # 10-bit input enabled.
    ## At this moment I can see the video 
    
    ## After each  of the next commands I do not see the video
    ## I tried them one by one and at any step the video was not converted, the screen was black
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x00 0x10 # PPL + DAC1
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x00 0x1C # PPL + all DAC
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x0D 0x0E
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x0D 0x06
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x0D 0x00
    root@j721s2-evm:/opt/edgeai-gst-apps# i2cset -y 1 0x2a 0x0D 0x08
    
    ##Disable PPL and  I see the video again
    i2cset -y 1 0x2a 0x00 0x12 # no PPL + DAC1

  • Hi,

      Kindly note that, for PAL operation an input clock of 29.5 MHz is required. If disabling the PLL solves your problem means, It indicates that the components used in the loop filter circuit need to be changed.
       You do need the correct loop filter components for the PLL. You can use a 169 1% resistor instead of 170 Ohms
    The loop filter requires these parts only.
    For the caps, It is suggested to use 150nF and 12nF 10% 25-50V NPO(C0G)
    For the resistor, It is suggested to use 169 Ohm 1%.

    If you are using the full temperature range, We would recommend using COG capacitors for their superior temperature performance.

    We do recommend the tight tolerances for the loop filter components to ensure the stability of the PLL.

    Thanks,
    Poornima
  • Hi,

    For reference, below you can see the schematic of how the chip is connected on our side.   

    For the caps, we use 150nF and 10nF. Is it a problem that we use 10nF instead of 12nF? 
    Could you also check if there is no problems with the connections in the schematic picture provided? 

    Regarding the clock:

    We provide a 27MHz clock as required for standard ITU-R BT.601/656 with a video resolution of 720x480.

    Also please note, that we provide ITU-R BT.601/656 video, but the register 0x80 is set to default value 0x10, meaning NTSC.

    Let me know if you need any additional information.

    Best regards,
    FoxFour

  • Hi,

      Kindly note that, When capacitance decreases from 12nf to 10nf then cut-off frequency of a External loop filter also decreases So use the filter components as per expert suggestion.

      Please crosscheck your schematic against our reference one at      6428.ADV739x_Evaluation_Board_Documents.zip

     By default, 0x80 register value is '0x10' If you are using PAL then configure that register as '0x11'.

    Thanks,
    Poornima
  • Hi,

    We tried to change to a 10nF capacitor but it did not help to enable PLL.
    The schematic looks good according to your reference.

    "Please crosscheck your schematic against our reference"
    We use NTSC

    Best regards,
    FoxFour

  • Hi,

    The ADV739x PLL only provides the oversampling clock.  Other then this the output is strictly based on your 27MHz incoming clock.

    on the ADV739x output, is the color burst stable and the right amplitude.

     can you attach a ntsc image with color problems?

    For ADV7393 are the EXT_LF components close to the part and the reference PVDD_1.8V supply very clean, especially when running ntsc?

    Normally these issues are related to poor color burst qualities and/or instability in the final NTSC signal.

    Thanks,

    Varshini K

  • Hi,

    - The colors look good on the test pattern.
    - I do not see any problems with the image color. The problem is that when I enable PLL the image stop streaming.
    - For ADV7393 the EXT_LF components are close to the part.
    - I checked the reference PVDD_1.8V supply and it looks good too.

    We assume that we have a defective ADV chip. We already ordered a new board sample. 
    It will take a long time for the new board to be manufactured.
    I will return with updates as soon as I get the new board.

    Best regards,
    FoxFour

Reply
  • Hi,

    - The colors look good on the test pattern.
    - I do not see any problems with the image color. The problem is that when I enable PLL the image stop streaming.
    - For ADV7393 the EXT_LF components are close to the part.
    - I checked the reference PVDD_1.8V supply and it looks good too.

    We assume that we have a defective ADV chip. We already ordered a new board sample. 
    It will take a long time for the new board to be manufactured.
    I will return with updates as soon as I get the new board.

    Best regards,
    FoxFour

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.