Post Go back to editing

EVAL-ADV7842-7511 Noise Interference lines

Hi, I have a EVAL-ADV7842-7511 Board which I'm using to decode CVBS signal from a Laserdisc player.

I have an issue where I'm seeing faint diagonal lines across the image. These are present on all of the input formats 10Bit, 24Bit and 36Bit and is also present on the s-video input. 

It it looks almost like interference. I've tried multiple cables and players and all produce the same results.

Any idea what is causing this?

many thanks

ken

Parents
  • I will confirm this but I believe they are static. Thin transultant diagonals. They are also not consistent and change in severity as I switch between input standards (10Bit, 24Bit, 36Bit) but it appears it's the switching of the input standard which Can affect it and not the specific input standard itself. 

Reply
  • I will confirm this but I believe they are static. Thin transultant diagonals. They are also not consistent and change in severity as I switch between input standards (10Bit, 24Bit, 36Bit) but it appears it's the switching of the input standard which Can affect it and not the specific input standard itself. 

Children
No Data