I have a question about the functions of the ADV7610.
We are currently considering using the ADV7610 for the following purpose in our newly designed system we are developing.
We plan to use the ADV7610 in the circuit configuration that receives HDMI signals sent from the CPU and sends YC signals and synchronization signals to the FPGA connected to the output side.
In this circuit configuration, the CPU sends a Vender Specific Info Frame (VSINF) packet to the ADV7610 at the beginning of each frame after Vsync. We think that the information in the VSINF packet is stored in the ADV7610 register and can be read via I2C, but after receiving VSINF, will the status be reflected in the register with almost no delay? How long is the delay until it is reflected in the register? Please let us know the recommended wait time for checking the state of VSINF.