ADV7280 Using interlaced output, all data is normal. After using the I2P function, use FREE-RUN, BOUNDARY BOX TEST PATTERN, It can be seen that the first and second rows sometimes have abnormal data, and the edges of the image appear to flicker. After using the PAL camera and I2P function, the image edges flicker. Not using I2P, using PAL camera, the image is also normal. The register configuration is from the official website, and the schematic diagram can be found on the official website. What could be the possible reason for this?