Post Go back to editing

ADV739x: Video Encoder outout circuit

Category: Hardware
Product Number: ADV739x

Hi,all.
we have question of ADV739x DAC output circuit.
Is it possible to use a circuit configuration like the following diagram, where a capacitor is inserted in series with the DAC output of the ADV7390?

best regards
AimPoint.

Parents
  • Hi,

      As per expert comment, We can use series capacitors to completely block the DC current flow through the signal path (The Cap is a DC blocking cap).

     The series capacitors block this DC offset and the input pin will bias the signal that is acceptable to the part.
     Also we can remove DC-Offset with a high-pass filter.

     Kindly refer here at (+) ADV7393: DC Offset on Output of DAC1 - Q&A - Video - EngineerZone (analog.com)

     Note: External filter and buffer components connected to the DAC outputs should be placed as close as possible to the ADV7390/ ADV7391/ADV7392/ADV7393 to minimize the possibility of noise pickup from neighboring circuitry and to minimize the effect of trace capacitance on output bandwidth. 

    Thanks,

    Poornima

Reply
  • Hi,

      As per expert comment, We can use series capacitors to completely block the DC current flow through the signal path (The Cap is a DC blocking cap).

     The series capacitors block this DC offset and the input pin will bias the signal that is acceptable to the part.
     Also we can remove DC-Offset with a high-pass filter.

     Kindly refer here at (+) ADV7393: DC Offset on Output of DAC1 - Q&A - Video - EngineerZone (analog.com)

     Note: External filter and buffer components connected to the DAC outputs should be placed as close as possible to the ADV7390/ ADV7391/ADV7392/ADV7393 to minimize the possibility of noise pickup from neighboring circuitry and to minimize the effect of trace capacitance on output bandwidth. 

    Thanks,

    Poornima

Children