Post Go back to editing

Digital to Analog conversion of progressive video of 640*480 by ADV7340/ADV7341 IP.

Category: Datasheet/Specs
Product Number: ADV7340/ADV7341, ADV7340

Thermal sensors generate the progressive video at a resolution of 640*480 and according to the ADV7340/ADV7341 datasheet, the video must be in an interlaced format to convert digital video of resolution 640*480 to analog video how to generate the analog output (NTSC and PAL) if the digital input is a progressive video of 640*480 by ADV7340/ADV7341 IP. 

Parents
  • Hi,

    ADV8005/ADV8003 is the only part which can support scaling as well as P to I conversation.

    This attached file ez.analog.com/.../adv739x-design-support-filesWhich ADV739x video encoder should I choose compares all members of the ADV734X and ADV739X series of parts.These are the latest video encoder parts on offer from ADI .

    Note: ADV7340/ADV7341 support an SD noninterlaced mode. Using this mode, progressive inputs at twice the frame rate of NTSC and PAL (240p/59.94 Hz and 288p/50 Hz, respectively) can be input into the ADV7340/ADV7341. The SD noninterlaced mode can be enabled using Subaddress 0x88 Bit 1. For more details please refer Page56 at ADV734x datasheet.

    Thanks,

    Poornima

Reply
  • Hi,

    ADV8005/ADV8003 is the only part which can support scaling as well as P to I conversation.

    This attached file ez.analog.com/.../adv739x-design-support-filesWhich ADV739x video encoder should I choose compares all members of the ADV734X and ADV739X series of parts.These are the latest video encoder parts on offer from ADI .

    Note: ADV7340/ADV7341 support an SD noninterlaced mode. Using this mode, progressive inputs at twice the frame rate of NTSC and PAL (240p/59.94 Hz and 288p/50 Hz, respectively) can be input into the ADV7340/ADV7341. The SD noninterlaced mode can be enabled using Subaddress 0x88 Bit 1. For more details please refer Page56 at ADV734x datasheet.

    Thanks,

    Poornima

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.