Post Go back to editing

ADV7535 resolutions

Thread Summary

The user inquired about the supported output video resolutions of the ADV7535, specifically if it supports VESA and SMPTE formats. The final answer indicates that ADV7535 queries should be directed to a private forum, and the engineer offered to send a private message to discuss the application further. The accompanying answer mentions that the ADV7535 supports video resolutions up to a maximum TMDS clock frequency of 148.5 MHz, which includes VESA formats up to that clock.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADV7535

Is there a table of output video resolutions supported by the ADV7535?  Does it support VESA and SMPTE resolutions?

Parents Reply Children