Post Go back to editing

Chip availability or chip detail for AHD converter

Thread Summary

The user inquires about AHD converters for MIPI DSI, HDMI, and LVDS inputs. The final answer confirms that no single-chip solution exists for MIPI DSI to AHD or LVDS to AHD. For HDMI to AHD, a two-chip solution is required: ADV761x/ADV784x for HDMI to pixel bus conversion and ADV800x for pixel bus to AHD conversion. The Serial Video Rx in ADV800x is designed for chip-to-chip connections and does not support direct HDMI input.
AI Generated Content
Category: Hardware

Hi ADI,

we are looking for AHD converter, If you have any converter with following specification
1. Mipi DSI to AHD
2. HDMI to AHD
3.LVDS to AHD 
etc ..
Parents
  • Hi  PoornimaSubramani 

    Good Day!

    What are the two chip which converter HDMI to AHD, Can you give me the Part number of them if possible give some design guidelines

    Thank you 

  • Hi,

     Kindly note that,We need to go for two chip solution for converting HDMI to Analog HD output. 

       ADV761x/ADV784x - It will convert HDMI to Pixel bus Output.

       ADV800x - It will take Pixel input to AHD Output.

    Here ADV761x converts input HDMI to Pixel port output and ADV800x takes the pixel port output of ADV761x as input and Outputs the AHD Video . For more information please refer the design support files of ADV761x and ADV800x.

    HDMI to Pixel bus converter
    Recommended for new design:
    ADV7842
    ADV7844
    ADV7610
    ADV7611
    ADV7612
    ADV7619
    Production:
    ADV7604
    ADV7614
    ADV7480
    ADV7481
    ADV7482
    Pixel bus to Analog HD
    ADV8005
    ADV8003
    Thanks,
    Poornima
  • Hi Poornima Subramani

    I go through  Datasheet of ADV8005/ 8003 there they mention we can provide HDMI input in Serial Video Receiver port, If there  why we need HDMI to pixel bus Converter first and then Pixel bus to HDMI converter, Instead of that we Directly give HDMI input to  ADV8005/ 8003 to get AHD output?. Can you please give me the clarity in that.

Reply
  • Hi Poornima Subramani

    I go through  Datasheet of ADV8005/ 8003 there they mention we can provide HDMI input in Serial Video Receiver port, If there  why we need HDMI to pixel bus Converter first and then Pixel bus to HDMI converter, Instead of that we Directly give HDMI input to  ADV8005/ 8003 to get AHD output?. Can you please give me the clarity in that.

Children