Hi ADI,
Hi,
Please find our response below,
1. MIPI DSI to AHD
None of our part can support MIPI to AHD Out.
2. HDMI to AHD
ADV7850 can support AHD to HDMI but we need to go for two chip solution to achieve 'HDMI to AHD'.
3.LVDS to AHD
None of our part can support LVDS to AHD.
Thanks,
Poornima
Hi Poornima
Can you please give the IC part number for Two chip solution for HDMI to AHD conversion
Hi PoornimaSubramani
Good Day!
What are the two chip which converter HDMI to AHD, Can you give me the Part number of them if possible give some design guidelines
Thank you
Hi,
Kindly note that,We need to go for two chip solution for converting HDMI to Analog HD output.
ADV761x/ADV784x - It will convert HDMI to Pixel bus Output.
ADV800x - It will take Pixel input to AHD Output.
Here ADV761x converts input HDMI to Pixel port output and ADV800x takes the pixel port output of ADV761x as input and Outputs the AHD Video . For more information please refer the design support files of ADV761x and ADV800x.
Hi Poornima Subramani
I go through Datasheet of ADV8005/ 8003 there they mention we can provide HDMI input in Serial Video Receiver port, If there why we need HDMI to pixel bus Converter first and then Pixel bus to HDMI converter, Instead of that we Directly give HDMI input to ADV8005/ 8003 to get AHD output?. Can you please give me the clarity in that.


Hi,
Kindly note that, It's not possible to achieve single chip solution with ADV800x part for 'HDMI to AHD' conversation Since Serial Video Rx accommodates inter-chip transfer of data over an HDMI compatible interface (for example, from an HDMI (Rx) such as ADV7850 or transceiver such as ADV7623).
Note: Serial video receiver is designed for chip-to-chip connection only and, as such, does not offer any DDC lines to facilitate HDCP or EDID operations so two chip is required for converting .
Thanks,
Poornima
Hi Poornima,
You have any EVK to convert HDMI to AHD for validation