I am using "MAX96724F-BAK-EVK#" with "LI-OV10635-GMSL" camera (which uses the "MAX96705 Serializer").


Best Regards,
Huy Huynh
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX96705
Not Recommended for New Designs
The MAX96705 is a compact serializer with features especially suited for automotive camera applications. It is function and pin compatible with the MAX9271...
Datasheet
MAX96705 on Analog.com
MAX96724F
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSLâ„¢2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724F on Analog.com


Hi,
As per below block diagram we can use 'MAX96705' as a serializer along with 'MAX96724F'.

Hello,
I am facing the same issue in GUI i am not able to see MAX96705. How do i configure the LI-AR0231-AP0200-GMSL2-060H camera with MAX96724F-BAK-EVK kit?
Hello,
I am facing the same issue in GUI i am not able to see MAX96705. How do i configure the LI-AR0231-AP0200-GMSL2-060H camera with MAX96724F-BAK-EVK kit?