Post Go back to editing

ADV7181C

here i attached design in file

please verify and give feedback

 

 

here are some clarification i need

 

in this design i used SDP 8-bit 4:2:2 mode

 

  1. for this mode the connections are right?

2.in this mode where i have to connect the following signals

   a.pin no#55  VS_IN

   b.pin no#56  HS_IN

   c.pin no#63  FIELD

   d.pin no#9  SFL/SYNC_OUT

   e.pin no#34  FB

   f.pin no#50  SOG/SOY

ADV7181C.pdf
Parents
  • 1) Watch the analog input impedance.  I don't see any 75 Ohm resistors or normal input circuit.  Please refer to the reference schematic in the data sheet.

    2) What are D1 & D2 for?

    3) ADV7181C is and old part, you should use ADV7181D

    Follow the reference circuit and you should be OK

Reply
  • 1) Watch the analog input impedance.  I don't see any 75 Ohm resistors or normal input circuit.  Please refer to the reference schematic in the data sheet.

    2) What are D1 & D2 for?

    3) ADV7181C is and old part, you should use ADV7181D

    Follow the reference circuit and you should be OK

Children
No Data