When we evaluated the ADV7610, unexpected LRCK output was observed after POR. We checked the Engineering Zone, but no similar questions were posted. At first, we would to clarify the behavior of LRCK clock after POR. We observed the following phenomena.
We captured the waveform of TDMS PLL lock output(Yellow) and LRCK output(Green). Regarding the LRCK output, 156kHz was first output after POR, and the LRCK output was switched to 96kHz at the timing of PLL locked, and then the LRCK was switched to 48kHz that we expected as proper audio clock. As for the parameter settings in the ACR packet receiving on the ADV7610, 48kHz clock is expected. It seems that the 156kHz LRCK clock is being output when the TMDS PLL is not locked. Is this correct behavior? We think that the LRCK should be determined from the frequency of the TMDS clock using the N and CTS parameters of the ACR packet in the TMDS.
Also, an unexpected clock output of 40.6kHz has been observed. Please let us know proper operation of LRCK output after POR, also please let us know if there is a way to prevent the 156kHz and 96kHz outputs, or if there is a proper procedure to set the frequency for LRCK audio clock output.

The ADV7610 D/S states a feature called Force_N_Update, The default setting of this bit is assigned to no effect . We think the N and CTS values should not be forcibly reloaded from the ARC packet under default configuration, we think 156kHz and 96kHz clock outputs we observed are not related to the Force_N_Update setting.