Post Go back to editing

MSEN state of ADV7625 TX.

Category: Hardware
Product Number: ADV7625

Please tell me about the MSEN state of ADV7625 TX.

When the MSEN state from the monitor is 0 with a metal wire HDMI cable, MSEN is incorrectly detected as 1 with an HDMI cable with EQ or an optical HDMI cable.

Some optical HDMI cables do not cause false detection and have an MSEN of 0.

So, my question is, which signal line is MSEN used to check? DDC line? TMDS line?

I would like to know how to identify optical HDMI cables that will not cause false positives like metal wires.

Best Regards.

  • Hi,

    On your prototype board try overriding HPD via HPD_OVERRIDE TX 0xD6[6].  Verify HPD is high by reading TX HPD_STATE 0x42[6]

    Also check RX_SENSE_STATE TX 0x42[5]

     

    When you see a high HPD, run the script and the output should go active.
     
    Thanks,
    Dharani S
  • Hello,

    MSEN stands for HDMI Clock termination.
    Does this signal become 1 when TMDS CLK is terminated and 0 when not terminated?

    For some optical HDMI cables and HDMI EQ cables, even if the SINK is not terminated, will it be terminated within the HDMI cable?

  • Hi,
     
    Monitor Sense detects the voltage level on the TMDS lines.  When it's ~2.5-3V it means the sink is connected and has the correct termination turned on.  The software checks this Monitor Sense bit and can decide to transmit or not.  Looks like the video card is doing the same thing.  It has to see a valid termination plus have a high HPD to begin transmitting.
     
    Many sources will not output TMDS unless they see the correct termination on the TMDS lines. First try with another source. Then let's see how you are setting TERM_AUTO  bits.
     
     
     
     
    rx_sense_pd should not  be applied  during the  configuration of  the HDMI  Tx as  it disables  an oscillator  required to  complete the  configuration of the TMDS output clock channel. It is recommended to use rx_sense_pd when the HDMI Tx has been completely configured. 
     
    Thanks,
    Dharani S