Post Go back to editing

ADV7280-M Timeout on Syncpt

I've recently posted about getting a ADV7280-M working over CSI on our NVIDIA Tegra system-on-module.

This now works and I can happily stream video.

However, I've recently stumbled across some issues when starting a gstreamer pipeline whereby occasionally, the video feed stutters and stumbles, with occasional half previous frames being shown alongside half current image frames (if that makes any sense).

Having had a look through the Linux dmesgs, I can see the following being output:

[ 1064.946867] vi vi: Timeout on VI syncpt
[ 1064.946891] vi vi: buffer_addr = 0x00707000
[ 1064.946911] vi vi: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000
[ 1066.956686] vi vi: Timeout on VI syncpt
[ 1066.956709] vi vi: buffer_addr = 0x0079f000
[ 1066.956750] vi vi: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000
[ 1068.956679] vi vi: Timeout on VI syncpt
[ 1068.956703] vi vi: buffer_addr = 0x00707000
[ 1068.956724] vi vi: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000
[ 1074.506788] vi vi: Timeout on VI syncpt
[ 1074.506812] vi vi: buffer_addr = 0x00707000
[ 1074.506833] vi vi: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000
[ 1076.516691] vi vi: Timeout on VI syncpt
[ 1076.516715] vi vi: buffer_addr = 0x0079f000
[ 1076.516736] vi vi: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000
[ 1078.516694] video4linux video0: Timeout on CSI syncpt
[ 1078.516719] video4linux video0: buffer_addr = 0x00707000
[ 1078.516744] video4linux video0: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000, ROSTATUS = 0x00000000
[ 1080.516752] video4linux video0: Timeout on CSI syncpt
[ 1080.516777] video4linux video0: buffer_addr = 0x00707000
[ 1080.516803] video4linux video0: PPSTATUS = 0x00000000, CILSTATUS = 0x00000000, ROSTATUS = 0x00000000

If I power down the camera and power back on while the gstreamer pipeline is closed, about 6/7 times out of 10, the video feed starts again and is smooth without stutter - the rest of the time, the feed is jerky and has issues (if I can capture some images then I will add them to this post).

One previous post on a similar "timeout on VI syncpt" issue mentions the "continuous_clk" field of the platform data for the camera. The adv7280-m driver on my Linux distro has it set to "1" which could be incorrect.

I'd be grateful for any advice.

Kevin

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.