I connected an OX05B OMS YUV camera to a MAX96712 using a MAX9295A deserializer. I found that the PCLK and video lock signals are normal, but the MAX96712 is not receiving any data. How should I troubleshoot this issue?
MAX96724
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSLâ„¢2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724 on Analog.com
I connected an OX05B OMS YUV camera to a MAX96712 using a MAX9295A deserializer. I found that the PCLK and video lock signals are normal, but the MAX96712 is not receiving any data. How should I troubleshoot this issue?
When I write the 0x40B register of max96712 as 0x02, I found 0x8d0 and 0x8d2 reported overflowed, why is that?
Hi,
Check the packet counter register on the deserializer for the data output. For example, check register 0x40 for the selected type Link A in the MAX96724 camera devices. Ensure that number of lanes, lane mapping, and routing of the data through video pipes are correct and that there are no errors on the serializer and deserializer. For display applications, if the sink is expecting a specific timing resolution, check that the source is providing that timing.
Currently only Maxim ATE products are supported on Engineer Zone at this time. Over the next several months, you will see more Maxim products being supported in Engineer Zone. Please visit one of the technical support pages on our newly integrated website below for assistance with Maxim Integrated products.
EN - https://www.analog.com/en/support/technical-support.html#
CN - https://support.analog.com/zh-CN/technical-support/
JP - https://support.analog.com/ja-JP/technical-support/
Thanks,
Dharani S
我正在使用max96712。我看到视频处于锁定状态,我可以在硬件上测量来自 max9295A 的数据,但 max96712 的测量始终处于较高水平。我尝试将0x40b写成0x02,但 max96712 报告再次溢出。我读0x8d0 0x10,0x8d2读0x11。如何解决此溢出问题?
我正在使用max96712。 我看到视频处于锁定状态,我可以在硬件上测量来自 max9295A 的数据,但 max96712 的测量始终处于较高水平。 我尝试将0x40b写成0x02,但 max96712 报告再次溢出。 我读0x8d0 0x10,0x8d2读0x11。 如何解决此溢出问题?
Hi,
For support regarding this product, please visit one of the technical support pages on our website below for assistance.
EN - https://www.analog.com/en/support/technical-support.html#
CN - https://support.analog.com/zh-CN/technical-support/
JP - https://support.analog.com/ja-JP/technical-support/