Post Go back to editing

To use AD9984A for coverting VGA signal to 24-bit RGB to the Microprocessor for further processing; which bits in the 30-bit RGB of AD9984A are to be discarded in schematic of hardware

Category: Datasheet/Specs
Product Number: AD9984A

I want to use AD9984A for coverting VGA signal to 24-bit RGB to the Microprocessor for further processing. Which bits in the 30-bit RGB of AD9984A are to be discarded in schematic hardware?

Whether AD9984A can be used for getting 24-bit RGB data? I want to store the input VGA to Microprocessor by converting to 24-bit RGB. Since AD9983A is going obsolete I cannot use in my new design. Hence AD9984A is planned to be used.

(Is this device suitable for VGA to 24-bit RGB conversion , if not please advice with any suitable Analog Devices IC)

Parents Reply
  • Hi Dharani,

    Thankyou for the support. I am planning to use AD9984A in 4:4:4 RGB (discarding LSBs:R0,R1,G0,G1,B0,B1) in schematics of hardware.

    I feel I cannot use ADV7401 and ADV7482 since its not the VGA resolution received over HDMI/DVI port that I need to process.

    Rather I need to convert the actual VGA connector port signals: the standard VGA pin-out signals(RGB+/-,Hsync,Vsync,SCL,SDA) to 24-bit RGB.

    Hence finalising on AD9984A. (Please correct me if I am wrong.)

Children