Post Go back to editing

Interfacing and synchronization

Category: Hardware
Product Number: ADV7125
Hi,
we are interfacing the ADV7125  DAC directly with i.MX6 CPU, the data is coming from i.MX6 CPU is in 24 bit 4:4:4 (RGB) format and Hsync and Vsync separately. 65MHz pixel clock frequency as shown in fig.
  
The question is, is it the proper way to interface.
second thing as the Hsync and Vsync are separately given to display, then how to  synchronize  Hsync and Vsync  with analog RGB signals.
Please give the proper solution for synchronize  of Hsync and Vsync  with analog RGB signals.
 
 
Regards,
Sanju

Thread Notes

Parents
  • Hi,

    The output wave forms are not dependent on BLANK or SYNC. BLANK and SYNC are just injected into the DAC outputs.
    Just watch the output amplitude to match the VGA input requirements. VGA requires separate 5V H & V sync signals.  You can still use the BLANK signal to blank the video during the refresh intervals. 
     
    The ADV7125 inserts timing information into the video to create the composite waveforms.

    In systems that utilize separate sync signals, synchronization is achieved by aligning the separate sync signals with the main video data. This alignment ensures that the display device knows when to start a new line (horizontal sync) and when to start a new frame (vertical sync), allowing for proper rendering of the video image.

    You can also refer ADV7123 and ADV7125 sync levels - Documents - Video - EngineerZone (analog.com) for sync levels.

     

    Thanks,
    Dharani S

Reply
  • Hi,

    The output wave forms are not dependent on BLANK or SYNC. BLANK and SYNC are just injected into the DAC outputs.
    Just watch the output amplitude to match the VGA input requirements. VGA requires separate 5V H & V sync signals.  You can still use the BLANK signal to blank the video during the refresh intervals. 
     
    The ADV7125 inserts timing information into the video to create the composite waveforms.

    In systems that utilize separate sync signals, synchronization is achieved by aligning the separate sync signals with the main video data. This alignment ensures that the display device knows when to start a new line (horizontal sync) and when to start a new frame (vertical sync), allowing for proper rendering of the video image.

    You can also refer ADV7123 and ADV7125 sync levels - Documents - Video - EngineerZone (analog.com) for sync levels.

     

    Thanks,
    Dharani S

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.