Post Go back to editing

ADV7511 fails in the system

Category: Hardware
Product Number: ADV7511

The customer uses ADV7511 for the DVI interface where they had some failures over the past few days. On all failed devices the customer can measure approximately 1 kOhm resistance between pin#35 and pin#42, TX0- and TX2- respectively. They have RClamp protection on these lines but still it is failing. What could be the reason for this issue? Thank you. 



Changed subject line from ADMV7511 to ADV7511
[edited by: mattp at 1:34 PM (GMT -5) on 16 Feb 2024]
Parents Reply Children