Post Go back to editing

[ADV7480] INTRQ2 setting

Category: Datasheet/Specs

Hi,

Customer has confirmed INTRQ1 and INTRQ2.
It was confirmed that INTRQ1 transitions from "H→L→H" in the sequence below.
However, INTRQ2 remains at H.

Are there any other settings required?

Initial setting        
  Dev_add Reg_add Write Val  
Write 0xE0 0x02 FF FF 0x00 0xE0 0xFF 0xFF  
Read 0xE0 0x01 47 0x01 0xE0 0x47   MPU_STIM_INTRQ_MB1
00    
Read 0xE0 0x01 46 0x01 0xE0 0x46   MPU_STIM_INTRQ_MB2
00    
Read 0xE0 0x01 40 0x01 0xE0 0x40   MPU_STIM_INTRQ
00    
Read 0xE0 0x01 41 0x01 0xE0 0x41   CP_LOCK_UNLOCK_EDGE_SEL
20    
Read 0xE0 0x01 45 0x01 0xE0 0x45   MPU_STIM_INTRQ_CLR
00    
Write 0xE0 0x1D 0x38 0xE0 0x1D 0x38 PDN_INT2
----------loop---------------    
Write 0xE0 0x02 41 24 0x00 0xE0 0x41 0x24 INT2_EN
Write 0xE0 0x02 46 02 0x00 0xE0 0x46 0x02 MPU_STIM_INTRQ_MB2
Write 0xE0 0x02 47 02 0x00 0xE0 0x47 0x02 MPU_STIM_INTRQ_MB1
Write 0xE0 0x02 40 04 0x00 0xE0 0x40 0x04 MPU_STIM_INTRQ
Read 0xE0 0x01 43 0x01 0xE0 0x43   MPU_STIM_INTRQ_RAW
42    
Read 0xE0 0x01 44 0x01 0xE0 0x44   MPU_STIM_INTRQ_ST
02    
Write 0xE0 0x02 40 00 0x00 0xE0 0x40 0x00 MPU_STIM_INTRQ
Write 0xE0 0x02 45 02 0x00 0xE0 0x45 0x02 MPU_STIM_INTRQ_CLR
Read 0xE0 0x01 43 0x01 0xE0 0x43   MPU_STIM_INTRQ_RAW
40    
Read 0xE0 0x01 44 0x01 0xE0 0x44   MPU_STIM_INTRQ_ST
00    
-----------------------------        

The register values actually confirmed by the customer are shown below.

Read E0 1D 0x01 #Setting_confirmation
78
Read E0 3F 0x0C #Setting_confirmation
3F 40 41 42 43 44 45 46 47 48 49 4A : Add
00 00 20 00 40 00 00 00 00 00 00 00 : Data
Write E0 1D 38 0x00 #1
Write E0 41 24 0x00 #2
Write E0 46 02 0x00 #3
Write E0 47 02 0x00 #4
Write E0 40 04 0x00 #5
Read E0 3F 0x0C #Setting_confirmation
3F 40 41 42 43 44 45 46 47 48 49 4A : Add
03 04 24 00 42 02 00 02 02 00 00 00 : Data
Read E0 43 0x01 #6
42
Read E0 44 0x01 #6
02
Read E0 3F 0x0C #Setting_confirmation
3F 40 41 42 43 44 45 46 47 48 49 4A : Add
03 04 24 00 42 02 00 02 02 00 00 00 : Data
Write E0 40 00 0x00 #8
Write E0 45 02 0x00 #7
./tp_i2c /dev/m_i2c1 0xE0 wr 0x01 43 0x01
Read E0 43 0x01
40
Read E0 44 0x01
00
Read E0 3F 0x0C #Setting_confirmation
3F 40 41 42 43 44 45 46 47 48 49 4A : Add
00 00 24 00 40 00 00 02 02 00 00 00 : Data
Read E0 1D 0x01 #Setting_confirmation
38
Read E0 3F 0x0C #Setting_confirmation
3F 40 41 42 43 44 45 46 47 48 49 4A : Add
00 00 24 00 40 00 00 02 02 00 00 00 : Data

Best regards.

Parents
  • Hi,

    From the shared settings, we inferred that the below settings to enable INTRQ2 are taken care of.

    INTRQ1 is always enabled, but INTRQ2 and INTRQ3 are disabled by default and must be enabled. INTRQ2 can be enabled by int2_en the control at Address 0x41[2].
     
    The power up status of ADV7480 at Address 0x1D[6]. Default status of intrq2 is Power down, we need to power up to change pdn_int2 to 0.
    This bit indicates the status of the interrupt signal on the INT2 interrupt pin. If an interrupt event that has been enabled for the INT2 pin has occurred, this bit will be set to 1. Interrupts for INT2 are set via the Interrupt 2 mask bits. This bit will remain set to 1 until all status for interrupts enabled on INT2 are cleared. So, make sure your previous interrupt was cleared or not by checking intrq2_raw.
     
    Also, please ensure with the below thing.
    The drive level of INTRQ1, INTRQ2 and INTRQ3 can be programmed independently as described here.
    Thanks,
    Dharani S
Reply
  • Hi,

    From the shared settings, we inferred that the below settings to enable INTRQ2 are taken care of.

    INTRQ1 is always enabled, but INTRQ2 and INTRQ3 are disabled by default and must be enabled. INTRQ2 can be enabled by int2_en the control at Address 0x41[2].
     
    The power up status of ADV7480 at Address 0x1D[6]. Default status of intrq2 is Power down, we need to power up to change pdn_int2 to 0.
    This bit indicates the status of the interrupt signal on the INT2 interrupt pin. If an interrupt event that has been enabled for the INT2 pin has occurred, this bit will be set to 1. Interrupts for INT2 are set via the Interrupt 2 mask bits. This bit will remain set to 1 until all status for interrupts enabled on INT2 are cleared. So, make sure your previous interrupt was cleared or not by checking intrq2_raw.
     
    Also, please ensure with the below thing.
    The drive level of INTRQ1, INTRQ2 and INTRQ3 can be programmed independently as described here.
    Thanks,
    Dharani S
Children
No Data