Post Go back to editing

EVAL-7613 AVES Blue Connection Settings

Category: Software
Product Number: ADV7613
Software Version: AVES Blue 3.03.1574

I am confused on how to connect to the EVAL-7613. 

What am I supposed to put here?

Thanks!

Parents
  • Hi,

    Please refer the document GettingstartedwithAVES.pdf at Advantiv Video Evaluation Software (AVESBlue).

    This pdf will give the details about how to connect the AVES with Eval board.

    If you are planning to connect to the evaluation board using a serial port then the appropriate driver for the USB to serial adapter must be installed. AVES verifies that is connected to the target through a special command sequence.

    And connect a RS232 cable directly to the board and select Advantiv Serial in the connection window. The program will search all COM ports for the right response.

    If you are going to use "ADS7 and SDP plugins" then you need to install SDP drivers. Download and install the SDP drivers as mentioned in GettingstartedwithAVES.pdf.
    Please get back to us if more clarification is required on this.
    Thanks,
    Dharani S
  • Hello,

    Where can I find the USB to serial adapter drivers?

    I have installed the SDP drivers. When I try to use the SDP Plugin, its looks like the EVAL-ADV7613 are custom. However, I do not have the number that needs to be input that corresponds with the EVAL-ADV7613.

    Could you kindly give me the number for the input where the arrow is pointing at.

    Also, maybe I am supposed to be using a Blackfin LDR, I don't not have the ldr file for the EVAL-ADV7613 though, is there a place I can find it?

    Thanks,

    OmuyaMHHT

Reply
  • Hello,

    Where can I find the USB to serial adapter drivers?

    I have installed the SDP drivers. When I try to use the SDP Plugin, its looks like the EVAL-ADV7613 are custom. However, I do not have the number that needs to be input that corresponds with the EVAL-ADV7613.

    Could you kindly give me the number for the input where the arrow is pointing at.

    Also, maybe I am supposed to be using a Blackfin LDR, I don't not have the ldr file for the EVAL-ADV7613 though, is there a place I can find it?

    Thanks,

    OmuyaMHHT

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.