Post Go back to editing

How to configure AP1 (Pin81) of ADV7671 as SPDIF audio output?

Thread Summary

The user inquires about configuring AP1 (Pin81) of the ADV7671 as an SPDIF audio output in their audio application setup. The final answer directs the user to contact VideoSupport@analog.com for detailed support, including configuration timing and supported frequency, bit number, and channel encoding format. The ADV7671 firmware version is 1.02-68612.
AI Generated Content
Category: Software
Product Number: ADV7671

Hello everyone
Our audio application plan is as follows:
PC ->HDMI interface ->ADV7671->SPDIF socket ->SPDIF to 3.5mm headphone box, both hardware and box are good. Now, the AP1 (Pin81) of ADV7671 is connected to the SPDIF socket on the hardware, so it is necessary to configure AP1 (Pin81) as SPDIF audio output; Please kindly provide suggestions on the specific configuration timing and the supported frequency bit number channel encoding format
ADV7671 firmware is 1.02-68612

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.