Hello all Members,
I own an EVAL-ADV7282A-M evaluation board. When I connect to the I2C pins via an external Initiator device (after desoldering resistors R17 and R18), which runs a frequency of 100kHz the chip is detected and responds to commands.
When I connect to the same pins with another I2C Initiator device, operating at a frequency of almost 400kHz - the chip does not respond.
What could be the cause?
The technical documentation allows an I2C bus clock of up to 400kHz.
I attach screenshots from the oscilloscope in two above scenarios.
www.analog.com/.../EVAL-ADV7282A-M.html


Please help to fix the problem.
Sylwester