Post Go back to editing

GMSL to SVGA conversion using ADV7125

Thread Summary

The user seeks to convert a GMSL video signal from a MAX9249 through an STP cable to SVGA using an adapter board. The final answer suggests using a MAX9276A deserializer to provide a parallel 24-bit RGB interface to the ADV7125 DAC, ensuring compliance with VESA standards and the desired SVGA resolution. The user confirms practical implementation and questions the resolution compatibility, which should be managed by the deserializer's correct configuration.
AI Generated Content

Hello ,

there is a need to convert gmsl video signal coming from max9249 through an stp cable to svga  with the use of an adapter board .
The SVGA should comply with:

  • VESA-2004-10 Video timing
  • VESA-2002-12 Signal definition
  • Comply VESA VSIS standard
  • RGB Outputs 0 to 0.7V
  • 800x600 @ 60, 72, 75, 85Hz non interlaced
  • HSync and VSync 3.3V (LVTTL/CMOS)

I searched a bit and I realized that I have to use a Video DAC for my purpose.
The solutions I found, for example the ADV7125, need parallel interface 24bit rgb inputs , so the signals must come directly from the deserializer if possible in the same interface.
There are some deserializers such as the max9276A, which seem to be able to deliver this interface.  So the idea is try to connect these 2 devices together.
The serializer of the other side(of which the gmsl signal comes from) is the max9249.
My question is if I miss something really crucial in this concept, for example can the ADV match the desired resolution of the svga, etc. etc., because this architecture seems to be at least HW-wise feasible.
Could you please help me?

Thank you very much in advance.

Edit Notes

title changed
[edited by: gkef at 9:14 AM (GMT -5) on 15 Dec 2023]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.