Post Go back to editing

MAX7301 digichain

Category: Datasheet/Specs
Product Number: MAX7301

I'm considering a digichain using three MAX7301s.
SCLK can only be sent up to 32 times (CS must be started once every 32 times)

So, is it possible to send the command in two parts as shown below?
(When transmitting for the second time, will 0x00, 0x03 written last time be output from DOUT from IC1, 2 to IC3?)

①CS UP→LOW
②Write 0x00,0x03 (32bit)
③CS Low→UP→LOW
④Write 0x02,0x01 (32bit)
⑤CS LOW→UP

(When transmitting ④, will 0x00, 0x03 written in ② be output from IC1, 2 to IC3 from DOUT?)



add comennto
[編集者:UBOTI、編集時刻: 11 Dec 2023 日 2:19 AM 時 (GMT -5)]
Parents Reply Children