Post Go back to editing

Is the GMSL input of the MAX9276A deserialiser compatible with the output of the MAX96705 serialiser?

Category: Hardware
Product Number: MAX96705,MAX9276A

The company for which I work is developing a deserialiser board based on the MAX9276A and am trying to test it with a camera based on the MAX96705.  I have not been able to detect a lock from the MAX9276A, and I was wondering whether these two chips are expected to work together.



tagged
[edited by: GenevaCooper at 11:08 PM (GMT -5) on 21 Nov 2023]