Post Go back to editing

Video signal input level and ferrite beads for power supply

Category: Datasheet/Specs
Product Number: ADV7391
Software Version: -

Hello.

I am considering adopting ADV7391BCPZ.

I have a few questions.

1.

I use the following power supply specs.

VDD_IO = 3.3V,  VAA = 3.3V,  VDD = 1.8V,  PVDD = 1.8V

 

Since VDD_IO = 3.3V, I plan to input 3.3V digital video signals to P0-P7.

Is my understanding correct ?

Or should I adjust the input level of P0-P7 to VDD's 1.8V ?

2.

I would like to know how to select the recommended components or constants for the fayrite beads to be inserted in the power supply line.

I will be using it in a circuit that inputs in ITU-R BT.656, 8-bit 4:2:2 YCrCb and outputs an analog signal in NTSC or PAL SD quality.

HSYNC and VSYNC pins are not used.

Regards,

Top Replies

  • FormerMember
    FormerMember
Oct 11, 2023 +1 verified

1) 3.3V digital inputs are good.  Check out Table 6 in the datasheet

2)  There are a number of good ways to implement the power rail filters.  The goal is to keep the power rails clean and isolated from each…

1) 3.3V digital inputs are good.  Check out Table 6 in the datasheet

2)  There are a number of good ways to implement the power rail filters.  The goal is to keep the power rails clean and isolated from each other.

  • The reference design uses Murata NFE61PT472C1H9L as part of the Pi EMI filter network
  • You can use ferrite beads such as Murata BLM15EG221SN1D.
  • I prefer Murata NFM21PC105B1A3D style filters.

  • Hi, GuenterL

    Thank you very much for your answer.