MAX96717
Production
The MAX96717 GMSL™ serializer receives video on an MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver. Simultaneously, it sends and...
Datasheet
MAX96717 on Analog.com
MAX96717F
Recommended for New Designs
The MAX96717F GMSL™ serializer receives video on a MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver. Simultaneously, it sends and...
Datasheet
MAX96717F on Analog.com
Hi, I'm trying to interface with GMSL2 solutions[MAX96717F-MAX96724F].
I need MAX96717 to generate 24MHz Clk to the image Sensor.
In MAX96717 datasheet, Reference Clock/DPLL Generation, it says that DPLL can be used to generate CLK which in range 1-75MHz.
Refer to max96717fr-user-guide, I wish to use this scenario. Using 25MHz Xtal / RoR is not be used
I found no more clue or guide to continue.
How Can I generate 24MHz CLK using DPLL?.
Which registers should I go to config? or which parameter need? If [fDPLL_OUT = (N.M)/K × fREF] is used, where should I found and assigned N M K?
Thanks,
Wipop