Post Go back to editing

Set the output image resolution of the ADV7511W chip.

Hi.

About the ADV7511W

The current status is that both the input and output image resolutions are 1024x768.

I want to change the output resolution to 720p (1280x720) without altering the input.

Is it possible to achieve this?

How can I do it?

Best Regard.

  • Hi,

      ADV7511 is just an HDMI transmitter. It has no memory and can't do any format or frame rate conversion but ADV8005 can do frame rate conversion as well Up/Down Scaling.
      Please note that ADV7511/ADV7513, the resolution that comes in is the resolution that goes out.

      This part does not have the ability to modify the resolution or the frame rate.

    Thanks,

    Poornima